Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Whats happening with EagleCad & Cadsoft?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 46 replies
  • Subscribers 191 subscribers
  • Views 5036 views
  • Users 0 members are here
Related

Whats happening with EagleCad & Cadsoft?

e14 Contributor
e14 Contributor over 15 years ago

HI,

 

There have been plenty of user suggestions (including myself ) over the

years and many relating to the same old issues.

 

As a PAYING User, I have essentially invested my money ( but a lot of my

time) into using & Learning EagleCad.

 

So..

 

I would like to know ( from the horses mouth if possible) what is Cadsoft

Proposing/Planning for the next release(s) of Eagle Cad?

Is there an advantage to anyone ( especially users) if future features are

kept secret?

 

The following is what I can see as major changes in no particular order and

not inclusive..

 

Q1) Are there going to be any major changes to the LIBRARY?

 

Q2) Are we going to have a proper user definable /properly integrated BOM

window ?

 

Q3) Can CUT, COPY & PASTE ( and selection/group) work just like any other

application?

 

Q4) Can we open more than one PROJECT or LIBRARY part at the same time?

Will we be able to copy and paste ( Drag and drop) between these?

 

Q5) Can all the user settings and scr files ( or whatever setting files) be

kept in just ONE FILE , in one place and All accessible in ONE User

Preference (TABBED) window? (we can get rid of the Control panel if we do

this, and it means that updating Eaglecad will be less painful).

 

Q6) Are their any plans for some sort of SChematic/Layout hierarchy or

SUB-Circuits feature.

 

Q7) Any plans for a built in Gerber Viewer ( mac users have almost nothing

to work with here?)

 

Q8) Any plans for built in Circuit Simulation ( even basic stuff)?

 

Q9) Any plans for The Built in text editor to have its own Syntax

Highlighting etc?

 

Q10) Any plans for a built in Gerber Panalizer/Merger Tool?

 

Q11) Are there any plans for more control over pads/holes in the device

editor? i.e Odd/Complex shapes.

 

Q12) Can the design link feature work with other suppliers. ( should be

part of the BOM System anyhow)

 

Q13) Can we place less reliance on ULP's and command line entries as a

source of features/enhancements or usability, this should really be only

for specialised tasks. If you have a look at the ULP's over the years

theres a ton of them for Library Management and BOM'S  Is that telling you

something?

 

Q14) Can we have single keystroke functions for at lease basic items, Move,

Change Layer, etc ( user definable of course).

 

I just want to know whats happening, The Beta Test forum is VERY QUIET, The

last release only really had Farnell Shopping added/improved and a few bug

fix's, I am worried that development has either slowed down or stopped. OR

is their  something big in the pipeline. ( hoping!)

 

I am also worried that most suggestions are "Frowned" upon and this really

puts new users off !

 

So that I , ( and everyone else ) can stop wasting our time ( and your

time) with suggestions, can you please answer or give us something to look

forward to?

 

One reason I am asking all the above is that I am considering spending a

LOT OF TIME learning the scripting language so that I can program my own

features ( I have lots of big ideas) , Why, Because I don't know what is

the future for Eaglecad, And I am concerned that I may get to the stage of

writing very useful ULP's and then Cadsoft will release something in the

near future that replaces my work. Remember that all the time I spend

learning the scripting language TAKES ME AWAY From designing boards and

managing production, which is what brings in the money! and besides I

really pay cadsoft for the programming expertise.

 

At the end of the day I believe Eaglecad has a lot of potential, while I

can get boards designed ( its all there as far as capabilities are

concerned) I just think that there are too many frustrating / cumbersome

ways of doing things when I know there are easier /better ways.

 

The designing of a schematic or Layout or even designing a library part is

quite easy ( once you finally figure out the Eaglecad way) , and yes this

is the main parts of an application like this. The issues are with the way

it all comes together or integrates and is managed and how the user

interacts with it. As I have stated above  the key issues are Mainly

Project management, BOM Management, and especially Libray Management.

 

Thanks for listening .

 

Dave M

 

PS Please don't condemn me for asking.

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Am 28.07.2011 00:32, schrieb davem:

    HI Andrew,

     

    yes there are plenty of MAC users in engineering, ( most of them keep quiet

    about it)  and yes Thanks to CADSOFT for having the balls for creating a

    Cross platform CAD application. The fact that Eaglecad exists on the mac

    help me decide to get into the electronics business, I think thats

    important. I have used mac's ( and PC's) since the Apple IIe?? ( Showing my

    age now!)

     

    >

    Thanks

    Dave M

     

    The whole discussion about the hardware is childish.

    This newsgroup is about eagle. So please everyone take your stupid bla

    bla about hardware elsewhere.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Hello everyone,

     

    Just to add to the cross-platform-ness of Cadsoft, they originally got me onboard because they had a

    version of Eagle that was built for OS/2.  Of course they discontinued that line, but given the

    direction the OS/2 software market was going, they had no choice.

     

    --

     

    Tony

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Hello everyone,

     

    Just to add to the cross-platform-ness of Cadsoft, they originally got me onboard because they had a

    version of Eagle that was built for OS/2.  Of course they discontinued that line, but given the

    direction the OS/2 software market was going, they had no choice.

     

    --

     

    Tony