EAGLE User Support (English) Creating a device from an existing symbol and package that are located in different libraries
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
  • Replies 2 replies
  • Subscribers 180 subscribers
  • Views 1410 views
  • Users 0 members are here
Related

Creating a device from an existing symbol and package that are located in different libraries

Former Member
Former Member over 14 years ago

Hi guys,

 

I'd like to create a new library part by combining a symbol and a package from already existing libraries.  The problem is that the symbol and the package are located in different libraries and I cannot seem to be able import them into the same library.  Is there any way to do that?  It might be a limitation but maybe I'm just a n00b.

 

Thanks,

Laci

  • Sign in to reply
  • Cancel
  • Richard_H
    Richard_H over 14 years ago

    Am 08.08.2011 14:26, schrieb László Monda:

    Hi guys,

     

    I'd like to create a new library part by combining a symbol and a package from already existing libraries.  The problem is that the symbol and the package are located in different libraries and I cannot seem to be able import them to the same library.  Is there any way to do that?  It might be a limitation but maybe I'm just a n00b.

     

    Thanks,

    Laci

     

     

    May I just copy from the manual.....

     

    Copy....

    From One Library into Another

     

    Devices

    If there is a proper Device or Device set that you want to use in

    your current library you can copy it in two different ways.

    In the Control Panel:

    Move (with Drag&Drop) the requested Device set from the Control Panel's

    tree view into the opened Library Editor window. The complete Device

    set with Symbol(s) and Package(s) will be copied and newly defined.

     

    As an alternative you could use the entry Copy to Library in the

    context menu of the Device entry.

     

    With the COPY command:

    Type, for example,

    COPY 75130@751xx.lbr

    or with the whole path

    COPY 75130@d:\eagle\lbr\751xx.lbr

    in the command line, the Device 75130 from library 751xx.lbr is copied into

    the currently opened library.

    If the path contains spaces use single quotes for it, for example:

    COPY '75130@d:\P A T H\751xx.lbr'

    If the Device should be stored in the current library under a new name simply

     

    enter it, like here:

    COPY 75130@751xx.lbr 75130NEW

     

     

     

    Symbols

    As Symbols are not shown in  the tree  view  of the Control Panel

    it is not possible to copy them from there into the Library Editor.

    Symbols are copied from one library into another the same way as one would

    do it within the same library. Therefore we use the commands GROUP, CUT,

    and PASTE.....

     

    The only difference to copying a Symbol within a library is that you have

    to open the other library (File/Open) after CUT and click into

    the group. Then you define a new Symbol that may have the same

    or another name as before.

     

    In short:

    • OPEN the source library and EDIT the Symbol

    • DISPLAY all layers

    • Select all objects with GROUP ALL

    • Use CUT and left mouse click into the group to set a reference point

    • OPEN your target library with File/Open

    • EDIT a new Symbol

    • Use PASTE to place it

    • Save library

     

     

     

    Package

    The procedure to copy Packages is nearly the same as to copy Devices.

    Either   move   (with   Drag&Drop)   the   requested   Package

    from   the   Control Panel's   tree   view   into   the   opened

    Library   Editor   window.   The   complete Package   will   be

    copied   and   newly   defined   in   the   current   library.

    As   an alternative you could use the entry Copy to Library

    in the context menu of the Package entry.

     

    Or use the COPY command. Type, for example,

    COPY DIL16@751xx.lbr

     

    in the command line, the Package DIL16 from library 751xx.lbr is

    copied into the   currently   opened   library.   If   the   library

    is   not   in   the   current   working directory you have to

    enter the whole path, as for example, in:

     

    COPY DIL16@\eagle\mylbr\751xx.lbr

     

    If the path contains spaces use single quotes for it:

     

    COPY 'DIL16@D:\P A T H \mylbr\751xx.lbr'

     

    If  the  Package should  be stored  in  the current library

    under  a new  name simply enter it directly in the command line:

     

    COPY DIL16@\eagle\mylbr\751xx.lbr DIL16NEW

     

    The Package is stored with the new name DIL16NEW now.

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago in reply to Richard_H

    Thanks a lot Richard, it works like a charm.