Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Re: Stop Mask for vias: two Limit fields   for top and bottom
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 206 views
  • Users 0 members are here
Related

Re: Stop Mask for vias: two Limit fields   for top and bottom

e14 Contributor
e14 Contributor over 15 years ago

I second this. Also, the info dialog with a via that has Stop on/off should

have tStop on/off and bStop on/off.

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    I second this. Also, the info dialog with a via that has Stop on/off should

    have tStop on/off and bStop on/off.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Bravo...   Having just upgraded to 5.11, I find that there are hundreds of Stop-Mask errors.  99.9% of all of the errors are USELESS.  I always use fairly large pads to allow for easy prototyping, production assembly and service repairs.  Since you do not easily allow for different pad sizes on the top and bottom of the board, I cannot make the top pad small and the bottom pad large to prevent the Silk Screen from overlapping large pads.

     

    I see no good reason why you even added these warning messages.  They do nothing to enhanse the error checking aspects of your package.

     

    Checking for Silk Screen violations around Holes is a good thing.  Checking for Silk Screen overlaps on Pads is worthless.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Bravo...   Having just upgraded to 5.11, I find that there are hundreds of Stop-Mask errors.  99.9% of all of the errors are USELESS.  I always use fairly large pads to allow for easy prototyping, production assembly and service repairs.  Since you do not easily allow for different pad sizes on the top and bottom of the board, I cannot make the top pad small and the bottom pad large to prevent the Silk Screen from overlapping large pads.

     

    I see no good reason why you even added these warning messages.  They do nothing to enhanse the error checking aspects of your package.

     

    Checking for Silk Screen violations around Holes is a good thing.  Checking for Silk Screen overlaps on Pads is worthless.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

     

    "jhannas@jrh1.us" <communitymanager@premierfarnell.com> wrote in message

    news:908973827.1281314167677998.JavaMail.jive@flmspu-csapp-02.premierfarnell.com...

    Bravo... Having just upgraded to 5.11, I find that there are hundreds of

    Stop-Mask errors. 99.9% of all of the errors are USELESS. I always use

    fairly large pads to allow for easy prototyping, production assembly and

    service repairs. Since you do not easily allow for different pad sizes on

    the top and bottom of the board, I cannot make the top pad small and the

    bottom pad large to prevent the Silk Screen from overlapping large pads.

     

    I see no good reason why you even added these warning messages. They do

    nothing to enhanse the error checking aspects of your package.

     

    Checking for Silk Screen violations around Holes is a good thing. Checking

    for Silk Screen overlaps on Pads is worthless.

     

    Its only useless if you dont use the silk when you manufacture the pcb. If

    you do, the silk gets printed onto the board and you dont want that printed

    on your pads!

    If you dont want to use it, hide the layer before doing DRC (and make sure

    the manufacturer doesnt print it).

    Optionally you may get the manufacturer to mask it with the pads, but thats

    is likely going to remove silk that you want to read.