Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Remember ALL window positions when QUITTING.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 188 subscribers
  • Views 1498 views
  • Users 0 members are here
Related

Remember ALL window positions when QUITTING.

e14 Contributor
e14 Contributor over 15 years ago

HI,

 

I am not sure if this has been asked before..

 

When opening EagleCad, the Control panel appears in the middle of the

screen. ( yep that's about it!)

 

I would like to have Eaglecad remember EVERY WINDOW and its POSITION SAVED,

when eagle cad quits. then when you re-open EagleCad, all your windows will

be as they were when you last left it!

 

Its very annoying at the moment..

 

especially when writing ULP's that I have to open a project ( for testing)

place it and resize it where I last left it.Open the help window, place it

and resize it where I last left it. reposition the Control panel resize it

where I last left it.open up my last ULP ( and maybe a few more), resize it

and position it. click though the menus of the control panel to find my

last project.. etc

 

this gets tedious.

 

I see no reason why, when eagle cad quits , it just records ..

 

1) The window(s) that were opened

2) The size of each window

3) the position of each window.

4) the stacking order

5) The current state of the hierarchy menus in the control panel.

 

This should be done for ALL windows ( including help, ulps, etc)

This should not effect anyones workflow, only improve it.

 

What do you guys think?

 

thanks

 

Dave M

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

     

    "Morten Leikvoll" <mleikvol@yahoo.nospam> wrote in message

    news:j327lf$ar9$1@cheetah.cadsoft.de...

    Except when you open the project saved on a huge double screen on a small

    laptop that will render the window outside.. But this is a special case

    and would need to reposition (like it currently does).

     

    If windows sizes would be saved proportional with desktop resolution, the

    problem you mentioned would not exist.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

     

    "Morten Leikvoll" <mleikvol@yahoo.nospam> wrote in message

    news:j327lf$ar9$1@cheetah.cadsoft.de...

    Except when you open the project saved on a huge double screen on a small

    laptop that will render the window outside.. But this is a special case

    and would need to reposition (like it currently does).

     

    If windows sizes would be saved proportional with desktop resolution, the

    problem you mentioned would not exist.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

     

    "jhannas@jrh1.us" <communitymanager@premierfarnell.com> wrote in message

    news:810198778.1271314167001173.JavaMail.jive@flmspu-csapp-02.premierfarnell.com...

    Gentlemen,

     

    There is only one problem with all of the suggestions so far. It is too

    easy to accidently hit the Close-Button at the top of the window. I have

    done it more than once when there are 200 windows open on the Desktop.

     

    I agree to that! image It would be nice to keep window settings even if you

    close one window.

     

    I cannot see any reason for discarding the window size and position

    information, EVER....

    Except when you open the project saved on a huge double screen on a small

    laptop that will render the window outside.. But this is a special case and

    would need to reposition (like it currently does).

     

    Either "ASK for verification of Close" when the Close-Button is clicked,

    or don't discard the windows parameters when a window is closed. If you

    want to be "backward-compatable", then also add a flag to the eagle.epf

    file, for the three possible windows, which preserves the window-state

    (minimized, normal, full).

     

    There should be a consistancy loss warning when closing one window. OR it

    should just hide the window when you close so that no consistancy gets lost.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Gentlemen,

     

    There is only one problem with all of the suggestions so far.  It is too easy to accidently hit the Close-Button at the top of the window.  I have done it more than once when there are 200 windows open on the Desktop.

     

    I cannot see any reason for discarding the window size and position information, at least for the Library, Schematic and Board information that is already in the eagle.epf file, EVER....  If you want to be "backward-compatable", then just add an (open, closed) flag to the eagle.epf file instead of discarding the valuable information that is contained in the project eagle.epf file.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Am 22.08.2011 11:42, schrieb Morten Leikvoll:

    "davem"<imix@bigpond.net.au>  wrote in message

    news:j2t5ji$v28$1@cheetah.cadsoft.de...

    >> Hi Morton,

    >>

    >> So how do you get those features you mentions to work?

     

    Create a project.

    Create your board and sch under the project (you can manually make a project

    by creating/copy the .epf file and open your brd/sch files after opening the

    proj)

    Use "open project"/"close project" instead of  window close!

    If you close a window manually, it will appear on a new pos when reopened

    (and you will loose new values entered in listboxes).

     

    This works with V5.11.0 and possibly with all V5's.

     

    >

    I close eagle with alt-x and don't have any problems.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Joerg wrote:

     

     

    >Another option is what I do: My PC goes to "Hibernate" instead of off.

    >So Eagle and all other programs are always exactly where they were

    >yesterday evening. Plus it starts a lot faster.

     

    Things can go wrong with hibernate, I disapprove your suggestion.

     

    Oliver

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Morten Leikvoll wrote:

    "davem" <imix@bigpond.net.au> wrote in message

    news:j2t5ji$v28$1@cheetah.cadsoft.de...

    >> Hi Morton,

    >>

    >> So how do you get those features you mentions to work?

     

    Create a project.

    Create your board and sch under the project (you can manually make a project

    by creating/copy the .epf file and open your brd/sch files after opening the

    proj)

    Use "open project"/"close project" instead of  window close!

    If you close a window manually, it will appear on a new pos when reopened

    (and you will loose new values entered in listboxes).

     

    This works with V5.11.0 and possibly with all V5's.

     

     

    Another option is what I do: My PC goes to "Hibernate" instead of off.

    So Eagle and all other programs are always exactly where they were

    yesterday evening. Plus it starts a lot faster.

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    "davem" <imix@bigpond.net.au> wrote in message

    news:j2t5ji$v28$1@cheetah.cadsoft.de...

    Hi Morton,

     

    So how do you get those features you mentions to work?

     

    Create a project.

    Create your board and sch under the project (you can manually make a project

    by creating/copy the .epf file and open your brd/sch files after opening the

    proj)

    Use "open project"/"close project" instead of  window close!

    If you close a window manually, it will appear on a new pos when reopened

    (and you will loose new values entered in listboxes).

     

    This works with V5.11.0 and possibly with all V5's.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Hi Morton,

     

    So how do you get those features you mentions to work?

     

    Dave M

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    "davem" <imix@bigpond.net.au> wrote in message

    news:j2shni$ecq$1@cheetah.cadsoft.de...

    HI,

     

    I am not sure if this has been asked before..

     

    When opening EagleCad, the Control panel appears in the middle of the

    screen. ( yep that's about it!)

     

    I would like to have Eaglecad remember EVERY WINDOW and its POSITION

    SAVED,

    when eagle cad quits. then when you re-open EagleCad, all your windows

    will

    be as they were when you last left it!

     

    Its very annoying at the moment..

     

    especially when writing ULP's that I have to open a project ( for testing)

    place it and resize it where I last left it.Open the help window, place it

    and resize it where I last left it. reposition the Control panel resize it

    where I last left it.open up my last ULP ( and maybe a few more), resize

    it

    and position it. click though the menus of the control panel to find my

    last project.. etc

     

    this gets tedious.

     

    I see no reason why, when eagle cad quits , it just records ..

     

    1) The window(s) that were opened

    2) The size of each window

    3) the position of each window.

    4) the stacking order

    5) The current state of the hierarchy menus in the control panel.

     

    This should be done for ALL windows ( including help, ulps, etc)

    This should not effect anyones workflow, only improve it.

     

    What do you guys think?

     

    It does save some of these today (control panel,sch,brd pos and size).. if

    you use projects. But remember many users work on several pc's with

    different screen properties (desktop, maybe even multiscreen,  laptop, etc).

    The issue has created a few support cases in time.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<