Hi Guys,
I'm having a problem with routing a board from a schematic. When I move
from the schematic to the board and use the auto router it connects wires
between pads and vias that it shouldn't. Eg. there are connections from the
annode to the cathode of some of the diodes. In the schematic there are no
connections between the two (no accidental wire running through the
component). The only thing is the schematic wires running over the top of
other wire and the software deciding that some of them are connected.
The ERC says everything is good though.
Is there a way that I can define a non-connection to be sure as this is a
big design involving multiple pics controllers and it would be almost
impossible to visually debug a routed board.
ALSO -I'm new to Eagle.
thanks in advance.
Darren,
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.