Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) 2 contractors, 64GB ram and 8 EC2 compute units and I STILL can't autoroute!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 190 subscribers
  • Views 675 views
  • Users 0 members are here
  • board
  • eagle
  • pcb_traces
Related

2 contractors, 64GB ram and 8 EC2 compute units and I STILL can't autoroute!

e14 Contributor
e14 Contributor over 15 years ago

Disclaimer - I'm the software guy, no the hardware guy)

 

Quick Deatils

  • Board is 11" x 11"
  • Contains two large BGA-like pad arrays, each with 364 pins
  • Contains ~580 parts
  • Board has 4217 connections

 

 

I've got quite the drama unfolding over here.

  1. We hired a contractor to do schematic capture and routing.
  2. He did the schematic and was into about 5 days of routing when he suggested to add two more layers to try to speed up the routing
  3. After adding the layers there was virtually no change
  4. We decided to move to another, more experienced contractor who also was going to make some vital circuit changes
  5. He made some additional schematic changes FAST and got right to routing
  6. After 2 days, the route job is still only at 93% (been there for about 12 hours now)
  7. He also asked for two more layers (now we're up to 8) and to drop the trace to .05mil
  8. It's STILL crawling
  9. I thought that eagle may be CPU/memory bound so I brought the most power Amazon EC2 Windows instance online (64GB ram and 26 compute units (30+ Ghz CPU power))
  10. I was shocked to see that Eagle only used one core and barely any ram and continued to drag along at an agonizing pace

 

At this point I'm getting desparate.  We have a HARD deadline coming up and if I don't come up with some gerber files in 3-4 days my project will be a disaster and could quite literally destroy my business.  I'm not being dramatic, it really could deal a death blow if we don't have this project ready for a trade show that's coming up.

 

So I wanted to ask the community here what ideas you may have for me?  A couple questions I have:

  1. Does the linux version of eagle utilize multiple cores/CPUs?
  2. Is the linux version native 64bit so it can use those 64GB of ram?
  3. Are the really expensive applications (OrCad) able to route circles around Eagle?  Should I jump my eagle ship and seek out a contractor with a higher-end toolset?
  4. If yes to #3, can the *.sch and *.brd files be imported into OrCad?

 

Please help.

 

-Steve

  • Sign in to reply
  • Cancel
Parents
  • Jorge_Garcia
    Jorge_Garcia over 15 years ago

    Hi Steve,

     

    This is Jorge Garcia of Cadsoft support.

     

    I can guarantee you that the problem lies with those BGAs, fanning out of a BGA is very difficult especially one with so many pins. I would recommend that you use micro vias and manually fan out from the BGAs; once you're out from under them the autorouter would be able to make relatively quick work of the rest of the board.

     

    To answer some of the questions you posted,the operating system has very little to do with the speed of the autorouter, EAGLE is exactly the same across all three major Os's. All of the muscle your machines have is futile because EAGLE can't make use of multiple cores(this is true of most commercial software today, parallization isn't the easiest thing to manage). Using another ECAD vendor's autorouter will only help if their autorouters are not grid-based; even that isn't a guarantee. Finally, there's no easy means to import EAGLE files into any other ECAD vendor (or vice versa) , there is a third party company that specializes in these types of conversions, but they can be a little pricey.

     

    Please e-mail support@cadsoftusa.com we'd like to see what we can do to get you out of your jam.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jorge_Garcia
    Jorge_Garcia over 15 years ago

    Hi Steve,

     

    This is Jorge Garcia of Cadsoft support.

     

    I can guarantee you that the problem lies with those BGAs, fanning out of a BGA is very difficult especially one with so many pins. I would recommend that you use micro vias and manually fan out from the BGAs; once you're out from under them the autorouter would be able to make relatively quick work of the rest of the board.

     

    To answer some of the questions you posted,the operating system has very little to do with the speed of the autorouter, EAGLE is exactly the same across all three major Os's. All of the muscle your machines have is futile because EAGLE can't make use of multiple cores(this is true of most commercial software today, parallization isn't the easiest thing to manage). Using another ECAD vendor's autorouter will only help if their autorouters are not grid-based; even that isn't a guarantee. Finally, there's no easy means to import EAGLE files into any other ECAD vendor (or vice versa) , there is a third party company that specializes in these types of conversions, but they can be a little pricey.

     

    Please e-mail support@cadsoftusa.com we'd like to see what we can do to get you out of your jam.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Jorge_Garcia

    Jorge_Garcia wrote:

     

    Hi Steve,

     

    This is Jorge Garcia of Cadsoft support.

     

    ....

     

    Please e-mail support@cadsoftusa.com we'd like to see what we can do to get you out of your jam.

    Hi Jorge,

     

    Thank you for the suggestions and comments.  I have just sent an email to support.

     

    -Steve