Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Allow trace routing to start anywhere
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 618 views
  • Users 0 members are here
Related

Allow trace routing to start anywhere

e14 Contributor
e14 Contributor over 14 years ago

Let me a bit more precise on this request: I mean anywhere where there is a reasonable location, i.e. a pad, via or already existing trace, so that Eagle knows what signal is being picked up fpr routing.

 

When routing traces on the PCB, one can only start routing where a rubber band/air wire starts. Quite often I find this bahavior coutner productive, as I would like to begin routing at some via on one end of the new trace, but the rubber band has attached itself to the closest location of another trace already routed to the end location. Therefore I am forced to begin routing at the inconvenient end. This is particularly troublsome when routing SMD devices with ICs where the pitch does not agree with the routing grid (which is practically always the case). To hit the IC pads exactly, one has to start routing at those pads. Often I find myself forced to rip up part of a trace, just so I can start routing where I need to.

 

Also it happens quite a bit that I would like to route an alternate track that seems to work out better, but only want to rip up the original trace once I get the new trace in and know that it works out. Same thing here, I have to rip up the original at least partly to be able to do any routing at all.

 

This restriction really gets in the way of productive work.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Element 14 User wrote on Sun, 02 October 2011 22:02

    When routing traces on the PCB, one can only start routing where a

    rubber band/air wire starts.

     

    Of course not, which even the quickest look at the documentation would have

    revealed.  This is mentioned at the top as the first entry in the section

    Mouse Keys.  It would have taken less time to type HELP ROUTE and find this

    than it did to whine here about not having this feature.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    On 10/02/2011 10:02 PM, egrom wrote:

    This restriction really gets in the way of productive work.

     

    see help route. Have you tried ctrl with route.  If a net still has an

    air wire then using ctrl when starting a route by clicking on pad or

    trace segment of the net will start a trace at or near your click.

     

    BTW this if from memory and version 4.1x.

    Paul R.