Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Automatic insert of jumpers
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 188 subscribers
  • Views 477 views
  • Users 0 members are here
Related

Automatic insert of jumpers

e14 Contributor
e14 Contributor over 14 years ago

I'm working on a simple schematic and, because I'll be etching the board

myself, I'm trying to keep the board single sided. Because it's single

sided the auto-router can do more than 90% of the routing, is it possible

to make eagle automatically add jumpers to complete the board? I can do

this manually, but is there a better solution?

 

Regards

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    I'm learning also but have found to produce a single sided board with wire

    links on the top you need to work as a 2 layer board; Follow the following

    extract and you will get the idea.

     

    Layers

    How do I make a single-sided PCB? Go into the Design Rule Checker (DRC

    tool), pick the Layers tab, and change the setup from (1*16) to 1. To

    change it back to a two-sided PCB, change the setup back to (1*16) and

    change the Nr 16 Copper back to .035mm.

     

    How do I make a single-sided PCB with a few jumpers? For home production of

    a single-sided board with a few component-side jumpers, make a two-sided

    board, only produce the bottom side, drill the vias as component pads [need

    to check what shows up in the drill file] and stuff jumpers where the

    top-side traces would go.

     

    How do I change layers while routing a trace? With a three-button mouse,

    use the middle button to change layers while routing traces. With a

    two-button mouse, click to set a waypoint, go up and change the layer in

    the drop-down box (don't worry about the weird rubber-band trace that

    follows your mouse around while you're doing it), and EAGLE should

    automatically insert a via, from which you can continue routing.

     

    How do I delete a via? Use the Ripup tool to delete vias. The X it leaves

    behind will disappear after the next routing operation (on that trace? at

    all?) or the next time you click Ratsnest.

    --

    Regards

     

    Ray B

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.