Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) CLI is faster than GUI myths
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 189 subscribers
  • Views 1512 views
  • Users 0 members are here
Related

CLI is faster than GUI myths

e14 Contributor
e14 Contributor over 14 years ago

Id like to start this thread to address the "CLI is faster than GUI" myths.

I challenge diehard CLI users to add their favorite command that they think

cant be done as efficient in a GUI, and I'll try to find a equally efficient

way to do it the GUI way.

 

Ill start adressing the group selection tool and the precision adjustment

myths.

 

A proper GUI would let you select the components you want to change with

either a select window drag (not having to activate the group) like a

powerpoint presentation design. It will also let you add and remove using

ctrl (or shift) selects like you do in a (win) filebrowser. Also, a filter

selection tool could help you add component based on name or other

parameters.

Then when right clicking one of the selected parts, it would pop up a

property window where all properties are presented (and props with different

values are marked as "dont change" by default), and it will give you the

option to overwrite them with a new value. All properties can be handled

like that, even fine positioning.

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Vom: Fri, 11 Nov 2011 10:59:31 +0100

     

    Hi,

     

    Id like to start this thread to address the "CLI is faster than GUI"

    myths. I challenge diehard CLI users to add their favorite command

    that they think cant be done as efficient in a GUI, and I'll try to

    find a equally efficient way to do it the GUI way.

     

     

    My challenge would still be the same as mentioned in the earlier thread:

     

    Take a large circuit with say, 500+ different signals. You got a "bus"

    of different signals, say OUT[0..255] and DATA[0..511].

    They are aligned in a complex way, so you can't select more than one

    signal with one click. Now you want to rip them up (and only them).

    I think the most efficient way would be "ripup OUT* DATA*;"

     

     

    Another challenge, apart from eagle, is this (not really serious):

     

    Receive an 8-bit digit X via UDP port 1000 and then draw a filled black

    circle with 50 pixel radius on position 5/15 into 3

    imagefiles /tmp/image[X].jpg, /tmp/image[X+1].png

    and /tmp/image[X+2].gif overlaying the previous image-content.

     

    Please don't nail me on this one, it's just an extreme example of

    an extraordinary special usecase where you have no chance with any GUI

    while you can do it extremly easy and quick with one line in a

    CLI/shell. (If you know how and don't have to learn everything

    first.) image

     

    It becomes more obvious when a task must be repeated

    oftenly. With a CLI you can just press <cursor-up> to redo (or

    copy/paste at least with any CLI). It has been mentioned that you can

    also assign a shortcut-key.

     

    Additionaly, eagle does it better than you: If you click-select you

    could easily miss a signal/part. If you say "LED*" then it really means

    every LED(...)-signal. So please don't see the CLI only as interface

    alternative, but also as a general principle of designing (which would

    prevent errors in this case). The best CLI is useless if your design

    is bad. For example, your naming doesn't make sense or your design is

    generally chaotic/unstructred.

     

     

    A proper GUI would let you select the components you want to change

    with either a select window drag (not having to activate the group)

    like a powerpoint presentation design. It will also let you add and

    remove using ctrl (or shift) selects like you do in a (win)

     

    ...or you can use a lasso-tool or "select-by-layer" etc. You could even

    have a mixture between GUI and CLI by providing sort of a tree-view of

    you whole project, showing all objects (signals, parts etc.) to

    perform different actions on (like scene-graphs known from 3D CGI

    Software).

     

     

    filebrowser. Also, a filter selection tool could help you add

    component based on name or other parameters.

     

    Yes. A filter would be a small LI inside a select-tool. This could

    support wildcards, patterns or even interpret regular-expressions.

     

     

    Generally, all you can answer to different challenges is inventing

    different GUI features that solve that challenge (more or less

    efficient).

    What you forget is, that someone has to implement that GUI feature

    (write code) and a decision must be made on how to implement it (GUI

    design).

     

    Excellent GUI design is far from beeing an easy task (obviously).

    In fact I have seen stuffed & un-intuitive GUIs that were so

    feature-rich trying to cover every possible use-case, that in the end

    they were almost unusable - although the underlying software was

    excellent (which was practically the only reason why someone decided to

    buy the software in the first place).

     

    Apart from the fact that designing a GUI is a never-ending task (since

    new features, that need a new kind of GUI interface, are added

    constantly) it is often overseen that a CLI is just a formal and

    structured representation of the programs' functionality.

     

    The programmer writes one piece of software (the parser) once. He never

    has to touch it again. It's finished. (Which is generally a good thing

    since no new bugs arise). New features don't need new parser code.

     

    This not only prevents bugs, but enables developers to quickly enhance

    functionality by extending the parser.

    Say for example the parser can parse something like " ...". After that, you implement wildcards or regular

    expressions etcetc.

     

    All those changes affect all possible commands (i.e. the whole

    functionality). The reasonable maximum amount of parser-features is

    limited, so that the parser-code is finished at some point, no matter

    how complex the parser is.

     

    I hope the advantage from the software-designers' & developers' point of

    view becomes clear. Additionally it's important to know that, if the

    software-design is good for developers the users directly profit from

    this in the form of less bugs, quick releases, more new features etc.

     

    But that's all theory. In reality your GUI must be "reasonable complete"

    to solve the most common tasks quickly since the majority of (new) users

    didn't (yet) learn the "structure" of the program or looked up CLI

    commands.

     

    Also, in reality new features always mean new GUI elements (CLI support

    or not). You still can run into the risk of an inefficient GUI. That is

    what somehow happened to Eagle. Additionally it can happen that the

    whole GUI must be completly re-designed at some point, forcing users to

    regain already learned knowledge.

     

     

    I think the whole point of the discussion is, that CLIs and GUIs are

    not opposing paradigms. Instead it's just 2 layers sitting ontop of the

    functions a software provides.

     

    So I really believe the one doesn't hurt the other but by providing an

    alternative to the GUI (be it ULP, Rexx, LUA, CLI, whatever...) a

    software can really unleash all its power in even the worst scenarios.

    Thusly more users are kept from getting frustrated since, in the worst

    scenario, you normally call for support. And it's better to get a

    10-page-instruction list that solves the problem than hearing "This

    just can't be done."

     

     

    And now for the sad part:

    In theory every software would be fine with a minimal, well designed

    GUI not implementing every feature but only the ones, you don't have a

    CLI alternative for (like visualization, mouse usage, etc.)

    So the GUI code would be finished at some point. Everything else would

    be controlled by CLI and the GUI code doesn't need to be touched when

    new features are implemented.

    This is of course a developers' dream and it pretty much was the way

    good software was designed decades ago. But times change image I guess the

    last CLI widely used by mainstream-users was the Hayes (AT) commandset

    for dialup-modems (using a terminal program as GUI frontend).

    So back in the days, users had to learn how to use a CLI but nowadays

    it's quite uncommon among most users. And since a CLI doesn't have a

    very steep learning-curve, lots of users try to avoid it wherever they

    can, thus never have the pleasure of advanced CLI features.

     

    This doesn't apply to Eagle alone but to most application-software and

    operating systems in general.

     

     

     

    many regards

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 12.11.2011 01:58, schrieb Daniel Hiepler:

    Take a large circuit with say, 500+ different signals. You got a "bus"

    of different signals, say OUT[0..255] and DATA[0..511].

    They are aligned in a complex way, so you can't select more than one

    signal with one click. Now you want to rip them up (and only them).

    I think the most efficient way would be "ripup OUT* DATA*;"

    Would be solved by the filter tool described below.

     

     

    It becomes more obvious when a task must be repeated

    oftenly. With a CLI you can just press<cursor-up>  to redo (or

    copy/paste at least with any CLI). It has been mentioned that you can

    also assign a shortcut-key.

    Many GUI tools have macro-recorders. Depending on the archictecture

    of an application, it's either easy to implement or unrealistic...

     

     

    Additionaly, eagle does it better than you: If you click-select you

    could easily miss a signal/part. If you say "LED*" then it really means

    every LED(...)-signal. So please don't see the CLI only as interface

    alternative, but also as a general principle of designing (which would

    prevent errors in this case). The best CLI is useless if your design

    is bad. For example, your naming doesn't make sense or your design is

    generally chaotic/unstructred.

    While we're at that:

    I want to manually re-number my components by clicking one component

    after the other.

    The current Eagle GUI does not support me much:

    If I want to name anything "R1", then I have to ensure first that no

    other component is named "R1".

    Then, when moving on to the next, I have to enter "R2".

    The result is that I don't clean up my component numbering....

     

    Is there a solution involving the CLI or a ULP?

    I see this thread also as CLI cookbook for the GUI users.

    But still, for such a standard task, no CLI should be required and

    I would expect the dialog box to have two checkboxes for what I want

    to accomplish.

     

    ...or you can use a lasso-tool or "select-by-layer" etc. You could even

    have a mixture between GUI and CLI by providing sort of a tree-view of

    you whole project, showing all objects (signals, parts etc.) to

    perform different actions on (like scene-graphs known from 3D CGI

    Software).

    Yes. A filter would be a small LI inside a select-tool. This could

    support wildcards, patterns or even interpret regular-expressions.

    +1 for tree and filter and also the rest of your post...

     

     

    Regards,

     

    Dietmar

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Dietmar Schwertberger schrieb:

     

    While we're at that:

    I want to manually re-number my components by clicking one component

    after the other.

    The current Eagle GUI does not support me much:

    If I want to name anything "R1", then I have to ensure first that no

    other component is named "R1".

    Then, when moving on to the next, I have to enter "R2".

    The result is that I don't clean up my component numbering....

     

    Is there a solution involving the CLI or a ULP?

     

    Maybe - I was already thinking about writing such a ULP (time permitted,

    and besides I fear that a ULP can't accept mouse clicks at all...).

     

    For the time being, I use renumber-sch-group.ulp - if you first renumber

    to a rather high starting index, you at least don't have any collisions

    at the lower when doing the final manual renumber.

     

    Besides, using the group functionality (rectangle area sorting), you can

    minimize the manual interactions to some degree.

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 12.11.2011 21:21, schrieb Tilmann Reh:

    Dietmar Schwertberger schrieb:

    >> While we're at that:

    >> I want to manually re-number my components by clicking one component

    >> after the other.

    >> The current Eagle GUI does not support me much:

    >> If I want to name anything "R1", then I have to ensure first that no

    >> other component is named "R1".

    >> Then, when moving on to the next, I have to enter "R2".

    >> The result is that I don't clean up my component numbering....

    >>

    >> Is there a solution involving the CLI or a ULP?

     

    Maybe - I was already thinking about writing such a ULP (time permitted,

    and besides I fear that a ULP can't accept mouse clicks at all...).

    Sounds good as temporary solution.

    But I assume that most users would not use/find it if the functionality

    is not included into the GUI.

    I would expect something like that in the Name dialog box:

      - "Auto increase" checkbox

      - "Resolve collisions" radio group or choice

        ("Inhibit", "Skip", "Rename other")

    Maybe a context sensitive toolbar could indicate whether the next number

    is available (green) or not (red).

    Maybe the two features could be integrated into the context sensitive

    toolbar.

     

     

    I was asking for a CLI solution as I seem to remember that there is one

    command which supports automatic numbering, but only in the CLI.

     

    For the time being, I use renumber-sch-group.ulp - if you first renumber

    to a rather high starting index, you at least don't have any collisions

    at the lower when doing the final manual renumber.

    As cleaning up is only 'nice to have' for my PCBs, that's already more

    work than I wanted to invest...

     

     

    Regards,

     

    Dietmar

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    I wrote:

     

    >> While we're at that:

    >> I want to manually re-number my components by clicking one component

    >> after the other.

    >> The current Eagle GUI does not support me much:

    >> If I want to name anything "R1", then I have to ensure first that no

    >> other component is named "R1".

    >> Then, when moving on to the next, I have to enter "R2".

    >> The result is that I don't clean up my component numbering....

    >>

    >> Is there a solution involving the CLI or a ULP?

     

    Maybe - I was already thinking about writing such a ULP (time permitted,

    and besides I fear that a ULP can't accept mouse clicks at all...).

     

    After thinking a short time about this, I posted a suggestion in a

    separate thread.

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    I wrote:

     

    >> While we're at that:

    >> I want to manually re-number my components by clicking one component

    >> after the other.

    >> The current Eagle GUI does not support me much:

    >> If I want to name anything "R1", then I have to ensure first that no

    >> other component is named "R1".

    >> Then, when moving on to the next, I have to enter "R2".

    >> The result is that I don't clean up my component numbering....

    >>

    >> Is there a solution involving the CLI or a ULP?

     

    Maybe - I was already thinking about writing such a ULP (time permitted,

    and besides I fear that a ULP can't accept mouse clicks at all...).

     

    After thinking a short time about this, I posted a suggestion in a

    separate thread.

     

    Tilmann