Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) EAGLE GUI (3): Unstructured menus
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 187 subscribers
  • Views 156 views
  • Users 0 members are here
Related

EAGLE GUI (3): Unstructured menus

e14 Contributor
e14 Contributor over 14 years ago

In our institute, the electronics workshop has a stock of several

thousand components, mainly distributed over a number of drawer

cabinets. To be able to find the components, the stock is structured

from the most general to the most detailed, and labelled accordingly.

 

The first cabinet is labelled 'Passive components', because that's

what's in there. There is NOTHING in there that is NOT a passive

component. That's clear and easy, and you cannot be mistaken.

 

The topmost x drawers are all labelled 'Resistors', each drawer with

some additional information like 'Resistors 1%, 1k-95k3, E48 series'. In

each of the resistor drawers, there is a maximum of 112 small boxes

containing all resistor values and labelled something like '1k, 1%,

0.6W, 100ppm, 300V' (or something similar). Below these 1% resistors,

there are 0.1% resistors. Below that, power resistors, special

resistors, several sorts of capacitors, coils, etc. All labelled

accordingly and CLEARLY. This way, you can easily and quickly find your

way through the stock and grab the necessary components.

 

Even people NOT overly familiar with electronics can find their way

through, because even these know the differences between 'passive

components', 'semiconductors', 'electromechanics' and 'mechanics'. There

are always some parts that will be tricky to find, but overall, it's

quite easy.

 

I COULD have structured the stock alphabetically, or by value (mixing

resistors, capacitors and coils and ONLY looking at their values), but

this would of course be completely ridiculous. For looking up a WORD in

a dictionary, alphabetical sorting is nice. For getting to know how to

DO things, it it NOT.

 

Unfortunately, EAGLE's menu bar is NOT properly structured, but

ALPHABETICALLY at points, which is extremely cumbersome and even

dangerous for new users. The 'Edit' menu contains lots of commands

sorted by their NAME. In my 'EAGLE GUI (2)' post, I already described

that using internal command names is a VERY BAD thing to do. Using more

descriptive (and clearer) texts, things can get MUCH easier to

understand, but the best thing is introducing STRUCTURE into menus:

Commands belonging together LOGICALLY should be near each other (NOT

alphabetically), helping the user guess HOW to do things.

 

CadSoft even did this properly at several points: E.g., UNDO and REDO

are NOT sorted alphabetically, but are next to each other. That's fine.

 

But why stop at that? All OTHER commands should ALSO be grouped

properly. In my 'EAGLE GUI (2)' post, I attached this horrific screen

shot of a schematics completely flooded with junctions, because the new

user didn't know the command NET, but used the obvious-sounding WIRE

instead (with all resulting problems). This is NOT only a problem of a

dangerously misnamed command, but also of NOT STRUCTURING the menu. If

the menu is NOT structured, the user just takes the command that SOUNDS

best. A structured menu gives the user additional hints about program usage.

 

Some commands in EAGLE support COMPONENTS, others ELECTRICAL

connections, still others create just graphics without electrical

function. THESE SHOULD ALL BE GROUPED for easy understanding.

 

Examples:

  - MOVE, ROTATE and MIRROR belong together, because they're all

    transformations.

  - REPLACE, GATESWAP and PINSWAP belong together, because they're

    all exchanging something that has to do with components.

  - NET, JUNCTION and BUS belong together, because they create

    ELECTRICAL connections.

  - In the schematics, WIRE, RECTANGLE, CIRCLE, ARC and POLYGON

    belong together, because they create GRAPHICAL objects. These

    should be SEPARATED from the electrical functions to prevent

    the mentioned disaster.

 

Additionally, think about better BALANCING your menus: EAGLE's

schematics editor uses 9 main menu entries, 5 of them having only less

than 5 entries. On the other hand, the EDIT menu is STUFFED with things,

even with ones NOT belonging there, e.g.:

  - ADD does not EDIT any already existing thing, but INSERTS

    something.

  - All four menu entries below VALUE are typically found under TOOLS

    (or something similar) in other software.

  - PASTE FROM is something that NOBODY will EVER search for in the

    EDIT menu. This is a FILE function usually called IMPORT. That

    EAGLE calls that by another name is bad enough, but completely

    leaving out the word FILE is unnecessarily ignorant of user

    interface standards.

Of course, EVERYTHING that the user can do SOMEHOW edits the design, but

this is NO reason to throw out all other menus and ONLY provide EDIT.

 

20 years ago, in bad old MS-DOS times, EAGLE didn't have ANY menu, just

text buttons. At that time, that wasn't so bad, because proper GUIs

still had to be invented, and all other programs were similarly cryptic.

In the meantime, GUIs have evolved and can now help the user

TREMENDOUSLY in learning unknown programs. EAGLE has implemented SOME

good interfaces (look at the NICE component previews during ADD, the

very useful CONNECT dialog and the ERC/DRC windows, all of which are

SUBSTANTIALLY better than), but MUCH to few.

 

In one recent post, one guy complained that the E in EAGLE stands for

'easy', but he couldn't really see that, because he found the interface

crappy. Though he complained about things that the program COULD do

properly (he just didn't know), he has a point: EAGLE's menu entries in

parts were taken over from a 20 year old piece of software, and haven't

evolved since. That's not nice. If CadSoft don't bring their interfaces

at least A BIT up to standard, EAGLE will lose ground with new users. We

don't want that.

 

In the next post, I'll try to give some example of how balanced,

structured menus with READABLE items might look.

 

Andreas Weidner