Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Strange Library behavior under Windows 7
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 188 subscribers
  • Views 563 views
  • Users 0 members are here
Related

Strange Library behavior under Windows 7

e14 Contributor
e14 Contributor over 14 years ago

I am running Eagle 5.11.0 under Windows 7 (64 bit)

 

Normally, under Windows 7, program files, such as the CadSoft supplied

".lbr" files are stored in

 

       C:\Program Files (x86)\EAGLE-5.11.0\lbr

 

If a user creates a new library, then Windows 7 puts it in

 

       C:\Users\\AppData\Roaming\CadSoft\EAGLE\lbr

 

I have my own custom libraries, so I put them in the appropriate AppData

folder.

 

Everything works fine until I download the latest SparkFun Eagle library.

 

If I put the SparkFun.lbr in the appropriate AppData folder then

Eagle can not see it.

 

If I put it in the appropriate lbr folder inside Program Files (x86)

then Eagle can see the library and all works fine.

 

What is different between all my other libraries and SparkFun.lbr that

it is not visible from the %appdata% folder?

 

I can override the Windows 7 security as a workaround, but why

does it not work like it is supposed to?

 

--- Graham

 

==

 

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    On 11/19/2011 6:37 PM, Graham wrote:

    I am running Eagle 5.11.0 under Windows 7 (64 bit)

     

    Normally, under Windows 7, program files, such as the CadSoft supplied

    ".lbr" files are stored in

     

    C:\Program Files (x86)\EAGLE-5.11.0\lbr

     

    If a user creates a new library, then Windows 7 puts it in

     

    C:\Users\<Name>\AppData\Roaming\CadSoft\EAGLE\lbr

     

    I have my own custom libraries, so I put them in the appropriate AppData

    folder.

     

    Everything works fine until I download the latest SparkFun Eagle library.

     

    If I put the SparkFun.lbr in the appropriate AppData folder then

    Eagle can not see it.

     

    If I put it in the appropriate lbr folder inside Program Files (x86)

    then Eagle can see the library and all works fine.

     

    What is different between all my other libraries and SparkFun.lbr that

    it is not visible from the %appdata% folder?

     

    I can override the Windows 7 security as a workaround, but why

    does it not work like it is supposed to?

     

    --- Graham

     

    ==

     

     

    Hi Graham,

     

    Windows 7 came out after the release of 5.11. At this moment Windows 7

    security features and EAGLE don't play very nice. The recommendation

    we're giving is to allow EAGLE to run in administrative mode,

    effectively over riding the security settings.

     

    This will be corrected for the release of version 6.

     

    Best Regards,

    Jorge

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Jorge Garcia wrote:

    Hi Graham,

     

    Windows 7 came out after the release of 5.11. At this moment Windows 7

    security features and EAGLE don't play very nice. The recommendation

    we're giving is to allow EAGLE to run in administrative mode,

    effectively over riding the security settings.

     

    This will be corrected for the release of version 6.

     

    Best Regards,

    Jorge

     

    --

    Come on Jorge get your information right.

     

    Windows 7 was General availablity October 22, 2009

    Eagle 5.11 was released  December 2010

     

     

    On that basis I would expect the Windows 7 problem to be fixed now for the

    final version of v5 (5.12) and the initial version of v6

     

    The excuses we are being subjected to have become  tiring.

     

    Warren

     

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 11/21/2011 5:58 PM, Warren Brayshaw wrote:

    Come on Jorge get your information right.

     

    Windows 7 was General availablity October 22, 2009

    Eagle 5.11 was released  December 2010

     

    >

    On that basis I would expect the Windows 7 problem to be fixed now for the

    final version of v5 (5.12) and the initial version of v6

     

    The excuses we are being subjected to have become  tiring.

     

    I'm only human Warren.

     

    Best Regards,

    Jorge

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 11/21/2011 5:58 PM, Warren Brayshaw wrote:

    Come on Jorge get your information right.

     

    Windows 7 was General availablity October 22, 2009

    Eagle 5.11 was released  December 2010

     

    >

    On that basis I would expect the Windows 7 problem to be fixed now for the

    final version of v5 (5.12) and the initial version of v6

     

    The excuses we are being subjected to have become  tiring.

     

    I'm only human Warren.

     

    Best Regards,

    Jorge