Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Grid unit /unitdist / dist
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 188 subscribers
  • Views 394 views
  • Users 0 members are here
Related

Grid unit /unitdist / dist

e14 Contributor
e14 Contributor over 14 years ago

The following correct behaviour seems to be a fault? (v5.11.2)

 

When I make changes to a grid unit and /or distance using the dialog and

then read the settings with UL_GRID,  I get results that are inconsistent..

 

 

 

Setting GRID from the command line it works as expected as described by HELP

(CORRECT BEHAVIOUR)

GRID mic 1000

Read with UL_GRID

UNIT = 0        (mic)

UNITDIST = 0        (mic)

DISTANCE = 1000

 

GRID mm

Read with UL_GRID

UNIT = 1        (mm as expected)

UNITDIST = 0         (mic)

DISTANCE = 1000

 

GRID mil

Read with UL_GRID

UNIT = 2        (mil as expected)

UNITDIST = 0         (mic)

 

 

GRID inch

Read with UL_GRID

UNIT = 3        (inch  as expected)

UNITDIST = 0         (mic)

 

 

 

Using the mouse and the GRID dialog I cannot get the above to happen

reliably (WRONG BEHAVIOUR)

 

I manually set GRID mic 1000

Read with UL_GRID

UNIT = 0        (mic as expected)

UNITDIST = 0        (mic as expected)

 

But if I return to the dialog and select INCH/OK

Read with UL_GRID

UNIT = 3        (inch  as expected )

UNITDIST = 3         (inch  was  NOT expected -should have remained as 0)

 

Starting again with

UNIT = 0        (mic as expected)

UNITDIST = 0        (mic as expected)

I return to the dialog and select MM/OK

Read with UL_GRID

UNIT = 1        (mm as expected)

UNITDIST = 0         (mic as expected)

DISTANCE = 1000

 

I return to the dialog and select MIL

Read with UL_GRID

UNIT = 2        (mil as expected)

UNITDIST = 2 (mil was NOT expected - should have remained as 0}

 

Some variations of the above do work correctly

 

I manually set GRID inch  0.01

Read with UL_GRID

UNIT = 3        (inch  as expected )

UNITDIST = 3         (inch  as expected)

 

I return to the dialog and select MM/OK

UNIT = 1       (mm  as expected )

UNITDIST = 3         (inch  as expected)

 

mil and mic  work OK in this direction as well

 

 

So an increasing UNIT has problems but a decreasing UNIT does not.

 

Warren

 

 

 

 

--

Viewed / responded via the newsgroup at

news.cadsoft.de

 

 

 

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    >

     

    I need to add to my previous post. While the behaviour was unexpected and

    was not mentioned in HELP, it does not result in misoperation. For those

    times when the UNITDIST was not as expected, the DIST was correct for the

    UNITDIST returned.

     

    Warren

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de