Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Scroll wheel with Eagle 6 on Mac
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 191 subscribers
  • Views 3210 views
  • Users 0 members are here
  • mac
  • zoom
  • mouse
Related

Scroll wheel with Eagle 6 on Mac

e14 Contributor
e14 Contributor over 14 years ago

Hi,

 

I've just upgraded to Eagle 6 (I'm looking forward to  indexing the XML format files for my search engine!) - however, I can't  get the scroll wheel to work.

 

It's enabled in the options (User Interface -> Mouse wheel zoom = 1.2), but it does absolutely nothing.

 

If I load Eagle 5.11, it works fine.

 

Note that setting the zoom to 0 doesn't allow me to scroll around either.

 

This happens with both of my mice (wired and wireless mighty mouse).

 

Any ideas?

 

BTW, I'm glad the bug where my ULPs to set the print zoom, mirror, black and so forth has been fixed since 5.11 - although I still can't use the Cmd-<n> keys to switch between the windows.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    I just installed Eagle 6.1 on my Mac (running Lion), and am very happy that pinch-to-zoom works now, and I can pan in Eagle!

     

    However, I often use an external mouse, without "pinch to zoom" functionality. I never liked the "legacy" mode, so I'm not willing to use that option, but I would like to be able to zoom with my external mouse.

    I would like to suggest the following: I have gotten very used to how Adobe allows zooming in the Creative Suite (I'm using version 3). While you press alt (option), and scroll, it zooms instead of scrolling. This would probably be a simple addition, and would greatly enhance usability when using an external mouse, and/or don't have pinch to zoom available.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    I'd like to second thefool's suggestion. I have an Apple Magic Mouse and would like to be able to scroll and zoom using the touch surface. Scrolling should be the default behavior, since it is consistent with mouse usage in other applications. Zooming should be accomplished through use of an option/alt key modifier as thefool suggests.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    I'd like to second thefool's suggestion. I have an Apple Magic Mouse and would like to be able to scroll and zoom using the touch surface. Scrolling should be the default behavior, since it is consistent with mouse usage in other applications. Zooming should be accomplished through use of an option/alt key modifier as thefool suggests.