Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Freerouting and Eagle V6
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 189 subscribers
  • Views 591 views
  • Users 0 members are here
Related

Freerouting and Eagle V6

e14 Contributor
e14 Contributor over 14 years ago

Note that I uploaded a new file to CADsoft (brd_to_dsn_V6.ulp) which

should replace the brd_to_dsn.ulp that arrived on the download site on

the 14th of December. The latter generates vias that are incorrectly

sized. Any ULPs that use absolute Eagle units should take into account

that the unit size changed from Eagle V5 to Eagle V6.

 

With brd_to_dsn_V6.ulp, Freerouting can be used to autoroute the board,

and generate the script to bring the layout back to Eagle V6.

 

I noted one issue though, related to using a .dru file from

Eurocircuits. In their .dru files they have the phrase:

 

"You can set the values for covered or “tented� via holes under

Masks (Limit)"

 

Whatever the characters are around "tented" they are replaced in in the

script file coming back from Freerouting as single quotes (') which

generates an error when opening the .brd file in Eagle. The solution is

to edit the .brd file, or better to modify the Eurocircuits .dru files.

 

Why this worked at all in Eagle V5 is not clear to me.

 

Robert Boers

 

 

  • Sign in to reply
  • Cancel
Parents
  • ameliaamelia
    ameliaamelia over 14 years ago

    Dear Robert,

    where is the"brd_to_dsn_V6.ulp"; I am not able to find it on ULP download.

    Amelia

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to ameliaamelia

    On 18/12/2011 01:55, ameliaamelia wrote:

    Dear Robert,

    where is the"brd_to_dsn_V6.ulp"; I am not able to find it on ULP download.

    Amelia

     

    Amelia,

     

    I uploaded it to CADsoft. I assume it will appear coming week in the

    download area (actually replace the earlier version that I uploaded).

    If you send me an email (robert at boers dot ch), I will send you a copy.

     

    Regards, Robert

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Hallo.

     

    I've found brd_to_dsn_v6.ulp at CADsoft, but I couldn't run it because of the syntax error at line 2 in it.

     

    Best regards. John.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Excuse me, I've used a wrong version of the script given at http://easyelectronics.ru/kasha-s-topora-na-bulone-iz-orla-primenyaem-topologicheskij-trassirovshhik-topor.html.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    On 31/08/2012 04:52, Evgeny Vaganov wrote:

    Hallo.

     

    I've found brd_to_dsn_v6.ulp

    (http://www.cadsoftusa.com/downloads/file/brd_to_dsn_v6.ulp) at

    CADsoft, but I could'nt run it because of the syntax error at line 2

    in it.

     

    Best regargs. John.

     

    John,

     

    I do not see an error in line 2. Can you show the line you have?

     

    Robert

     

    NB I am testing a slightly modified version that generates more

    efficient DSN code for curved lines. Will publish that in a few days,

    but that should not change the error you report.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    On 31/08/2012 04:52, Evgeny Vaganov wrote:

    Hallo.

     

    I've found brd_to_dsn_v6.ulp

    (http://www.cadsoftusa.com/downloads/file/brd_to_dsn_v6.ulp) at

    CADsoft, but I could'nt run it because of the syntax error at line 2

    in it.

     

    Best regargs. John.

     

    John,

     

    I do not see an error in line 2. Can you show the line you have?

     

    Robert

     

    NB I am testing a slightly modified version that generates more

    efficient DSN code for curved lines. Will publish that in a few days,

    but that should not change the error you report.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Excuse me, I've used a wrong version of the script given at http://easyelectronics.ru/kasha-s-topora-na-bulone-iz-orla-primenyaem-topologicheskij-trassirovshhik-topor.html.