Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Running the CAM processor from the command   line
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 188 subscribers
  • Views 1904 views
  • Users 0 members are here
Related

Running the CAM processor from the command   line

e14 Contributor
e14 Contributor over 14 years ago

I just lost a few days on a board due to my being in a hurry.  Does anyone

know how to run the "drillcfg.ulp" and then start-up the CAM processor to

do the rest of the steps???  Or, is there a way to bypass the step to run

the drillcfg.ulp??  I have searched the HELP for running the CAM from the

command line, although, every other conceivable command is in there, where

is CAM???

 

Thanks for the help.

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Stewart wrote:

    I just lost a few days on a board due to my being in a hurry.  Does

    anyone know how to run the "drillcfg.ulp" and then start-up the CAM

    processor to do the rest of the steps???  Or, is there a way to

    bypass the step to run the drillcfg.ulp??  I have searched the HELP

    for running the CAM from the command line, although, every other

    conceivable command is in there, where is CAM???

     

     

    The term 'command line' refers to two uses. One is within Eagle and is the

    command line you see in each editor window. The other is outside of Eagle.

    It refers to launching applications from a command window or terminal

    window.

    You cannot run the CAM by typing into the editor command line. You need to

    click the CAM icon on the toolbar or select from the drop down menus

    File/CAM Processor. Using the keyboard you could type Alt-F followed by

    Alt-M.

     

    You can launch Eagle with command line parameters which  tell it to run the

    CAM processor (command line method) which is useful for scripts and ULPs. I

    suspect this is not what you are after.

     

    Warren

     

     

     

     

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Warren,

    Thanks for your reply.  As I thought I had made clear, I want a one command

    solution to generating GERBERS and drill information.  I want to automate

    the process so that none of the currently required 3 steps get forgotten in

    the current manual process.  I want to do a script/ulp that does the whole

    thing, that is run the CAM after the drillcfg has been done.  I did add the

    settings from "excellon" to my list of job file configurations. Which, now

    I am down to 2 steps, just need to get it down to ONE STEP.  (and of course

    I want to do this in the layout editor, not as a command line parameter

    during the launch of Eagle from the desktop)

     

    Stewart

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Stewart wrote on Thu, 29 December 2011 19:56

    As I thought I had made clear, I want ...

     

    People often ask for the wrong thing or something unreasonable.  Other than

    the Cadsoft folks who do chime in here on occasion, the rest of us are free

    to answer whatever parts of a question we think is worth it, have time for,

    know the answer to, or otherwise just feel like.  Sometimes that means

    answering a different question that we think is more relevant.  That's how

    peer to peer support works.

     

    Quote:

    a one command solution to generating GERBERS and drill information.

     

    You can possibly do this with the information Warren gave you, although

    this one command will be difficult since there are various options in the

    process.

     

    Quote:

    I want to automate the process so that none of the currently required 3

    steps get forgotten in the current manual process.

     

    First, it's more than three steps.  Second, this is only once per board, so

    you're not going to get much return for taking the time to make this a

    automated process.  I have thought about this myself and decided it's not

    worth it.

     

    Instead, I use a checklist.  I have a script that gathers all the various

    files required by a board house into one zip file.  The checklist is in the

    comments of that script:

     

     

    rem   The steps in creating the right files in Eagle from a completed

    rem   board layout are:

    rem

    rem   1  -  Make sure there are fiducials in two opposite corners.

    rem

    rem   2  -  Add the layer name to each layer outside the board area.

    rem

    rem   3  -  Run DRILLCFG.ULP from the board editor.  Specify inches.

    rem         Go back and fix hole sizes that aren't in the

    ~/eagle/holes.txt

    rem         list.

    rem

    rem   4  -  Run the EXCELLON.CAM CAM processor job to create the

    rem         drill data (.DRD) file.

    rem

    rem   5  -  Run the Generic2L (2 layer boards) or Generic4L

    rem         (4 layer boards) CAM processor jobs.  This will produce the

    rem         gerber files for each photo-plotted layer.

    rem

    rem         NOTE 1: Delete the solder paste mask output file(s) if package

    rem           is for PCB only, not full board manufacturing.

    rem

    rem   8  -  Run this script to create the ZIP file with all the needed

    rem         files.

    rem

    rem   7  -  Visually verify the Gerber files with a Gerber file viewer.

     

    The whole script is included in my Eagle Tools release at

    http://www.embedinc.com/pic/dload.htm

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Stewart wrote on Fri, 30 December 2011 13:34

    I also agree that the generation of GERBERS should only happen once per

    board revision, but in the real world, this process may occur several

    times during the course of improvements.

     

    Sure, but the process is still small compared to each chunk of work that

    results in you needing new gerber files.  It takes maybe a whole minute

    (I'm being pessimistic) to generate the CAM files for a board.  At best

    automating this will save that minute once every time you make new files,

    each of which probably represents at least a hour or more of work.

     

    There are more productive things to chase aftere to improve. 

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Stewart wrote on Fri, 30 December 2011 13:34

    I also agree that the generation of GERBERS should only happen once per

    board revision, but in the real world, this process may occur several

    times during the course of improvements.

     

    Sure, but the process is still small compared to each chunk of work that

    results in you needing new gerber files.  It takes maybe a whole minute

    (I'm being pessimistic) to generate the CAM files for a board.  At best

    automating this will save that minute once every time you make new files,

    each of which probably represents at least a hour or more of work.

     

    There are more productive things to chase aftere to improve. 

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.