Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Quirky bug in 6.x
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 188 subscribers
  • Views 224 views
  • Users 0 members are here
Related

Quirky bug in 6.x

e14 Contributor
e14 Contributor over 14 years ago

Hi,

 

I have found a small bug between 5.11 and 6.1, surrounding a slightly

eccentric technique I use for component management.

 

I have a device in one of my libraries which contains only a ">Value"

label in both the symbol (on the "Values" layer) and the package (on

"Document" layer).  It has no pins, no lines, no ">Name" text.  The

device has a user-selectable value.

 

The reason I made this device is so that I can add components not

otherwise represented on the PCB layout (connecting wires, jumper

blocks, enclosures, etc) complete with attributes like supplier order codes.

 

The benefit of this is that I can add several of these "OFFBOARD"

components to my schematic, complete with values like "USB A-to-B

cable", "1A 20mm fuse" and so on.  The result is a note on the schematic

(and on the PCB layout) of components not otherwise shown, as well as

lines in the ULP-generated Bill of Material containing those devices and

their order codes right along with all of the other components.

 

There's probably a better way of doing this (and I welcome suggestions)

but, in any event, it has shown up a bug:

 

In 5.11 my OFFBOARD component works as expected.  Now, in 6.1 (and all

6.x versions) the value assigned to the component is shown on the PCB

but not on the schematic unless:

 

1. The part is SMASHed OR

2. The part is modified to include a ">Name" (which I'd raher not have)

 

This is hardly an urgent bug, since it's rather a rather unusual

use-case and simply SMASHing the part works around the problem, but

please add it to the list in case it's a symptom of something nastier.

 

A library containing the offending component is attached.  Unfortunately

I now only have this in v6.x format.

 

All the best,

 

 

 

Andrew

0xADF

 

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    On 13/01/12 16:18, Andrew Feldhaus wrote:

    Hi,

     

    I have found a small bug between 5.11 and 6.1, surrounding a slightly

    eccentric technique I use for component management.

    >

    > 8<--- snip

     

    Actually scratch that.

     

    I can't reproduce the bug on 6.1 under Linux x64 -- I suspect I may have

    been doing something stupid.

     

     

    Andrew

    0xADF