Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Addition of a new standardized font
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 187 subscribers
  • Views 1176 views
  • Users 0 members are here
Related

Addition of a new standardized font

e14 Contributor
e14 Contributor over 14 years ago

Hi

In general I think that the Eagle approach to limit the number of available fonts is a good one since it makes it much easier to get a consistent appearance of the symbols in the libraries.

However I think that the collection of fonts is too limited at the moment.

 

I think that a logical step in the development of Eagle would be to include a new standardized font, such as the osifont (http://code.google.com/p/osifont/).

Schematics designed with this font will be accepted by customers requiring the use of fonts according to ISO3098, for instance by requiring fulfilment of IEC61082.

 

Besides that technicality, osifont is free and it is designed to be readable.

 

Kind Regards

Anton Andersson

Sweden

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    antan951 wrote:

     

    Hi

    In general I think that the Eagle approach to limit the number of

    available fonts is a good one since it makes it much easier to get a

    consistent appearance of the symbols in the libraries. However I think

    that the collection of fonts is too limited at the moment.

     

    I think that a logical step in the development of Eagle would be to

    include a new standardized font, such as the osifont

    (http://code.google.com/p/osifont/). Schematics designed with this font

    will be accepted by customers requiring the use of fonts according to

    ISO3098, for instance by requiring fulfilment of IEC61082.

     

    Besides that technicality, osifont is free and it is designed to be

    readable.

     

    Kind Regards

    Anton Andersson

    Sweden

     

    I think thas is a good idea, and a good choice of font.

     

    --

    Morgan Leijström, Tribun AB

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Morgan Leijström schrieb:

     

    >> I think that a logical step in the development of Eagle would be to

    >> include a new standardized font, such as the osifont

    >> (http://code.google.com/p/osifont/). Schematics designed with this font

    >> will be accepted by customers requiring the use of fonts according to

    >> ISO3098, for instance by requiring fulfilment of IEC61082.

    >>

    >> Besides that technicality, osifont is free and it is designed to be

    >> readable.

     

    I think thas is a good idea, and a good choice of font.

     

    I fully agree with this (both).

     

    This request is very long-standing, BTW... (Previously, Hershey fonts

    have been suggested, which is quite similar.)

     

    Tilmann

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 19.01.2012 12:47, schrieb Tilmann Reh:

    This request is very long-standing, BTW... (Previously, Hershey fonts

    have been suggested, which is quite similar.)

     

    When implementing new fonts, one should always consider WHAT these fonts

    should be used for:

      1. The suggested TrueType font is very useful for SCHEMATICS,

         because it's both readable and technical.

      2. For BOARDS, however, a font is needed that can easily be

         sent to a whole range of sophisticated output devices, like

         'normal' printers, HPGL plotters, Postscript files, Gerber

         devices, etc. This can NOT be properly done with such

         TrueType fonts.

      3. The same is valid for the TrueType (or other outlined

         font) technology in general: Depending on the operating

         system and its current font engine implementation, the

         actual rendering of text will be DIFFERENT in size,

         leading, width, etc. The differences here are so small that

         they should not matter too much in the schematics, but on

         board they might be the reason why copper pour changes,

         so that unconnected islands appear or other stuff like that.

      4. In order to have the board behave COMPLETELY reliable,

         so-called VECTOR fonts (or stroked fonts) need to be used,

         which is why I proposed the Hershey stuff long time ago.

     

    Therefore: The TrueType font IS nice, but just cannot be used for the

    board. A better STROKED font is needed for that.

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Tilmann Reh wrote on Fri, 20 January 2012 05:26

    The suggested font appears exactly like the previously suggested (by

    you, as well as by me) hershey font. I don't know how/if this font can

    be "vectorized" as well,

     

    The Hershey fonts are vector.  However, instead of Cadsoft picking and

    imposing fonts on us, they should publish a font file format and allow us

    to tell Eagle what font to use.  Converting the Hershey fonts, or any other

    vector fonts, to whatever format Cadsoft decides should be easy.

     

    Along with that they should allow some way of specifying arbitrary

    character codes in the text command so that we can access non-ASCII

    characters at unused character codes of our chosing.  My graphics programs

    generally use vector fonts, and I have added non-ASCII symbols I

    occasionally use for some of the unused character codes 0-31.  For example,

    the upper case omega is code 7 and lower case micron code 3.  I don't

    expect, nor want, Cadsoft to provide anything more than the standard

    character set.  As long as we can define our own fonts, that's no problem.

    I'd probably write a program to convert my modified Hershey simplex.h font

    to Cadsoft's format and not look back.

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Tilmann Reh wrote on Fri, 20 January 2012 05:26

    The suggested font appears exactly like the previously suggested (by

    you, as well as by me) hershey font. I don't know how/if this font can

    be "vectorized" as well,

     

    The Hershey fonts are vector.  However, instead of Cadsoft picking and

    imposing fonts on us, they should publish a font file format and allow us

    to tell Eagle what font to use.  Converting the Hershey fonts, or any other

    vector fonts, to whatever format Cadsoft decides should be easy.

     

    Along with that they should allow some way of specifying arbitrary

    character codes in the text command so that we can access non-ASCII

    characters at unused character codes of our chosing.  My graphics programs

    generally use vector fonts, and I have added non-ASCII symbols I

    occasionally use for some of the unused character codes 0-31.  For example,

    the upper case omega is code 7 and lower case micron code 3.  I don't

    expect, nor want, Cadsoft to provide anything more than the standard

    character set.  As long as we can define our own fonts, that's no problem.

    I'd probably write a program to convert my modified Hershey simplex.h font

    to Cadsoft's format and not look back.

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.