Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Re: Multiple gate trouble when creating part in library
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 187 subscribers
  • Views 190 views
  • Users 0 members are here
Related

Re: Multiple gate trouble when creating part in library

e14 Contributor
e14 Contributor over 14 years ago

Am 27.01.2012 22:29, schrieb rickford66:

Hi,

I've created a dozen or so parts in libraries so far and, with a little help from the manual, youtube, and this forum, have had great success.  Now I'm trying to create a part with multiple "gates".  It's an 8 pin dual n-channel MOSFET.  I want the MOSFETs to be independent (A and B) like a regular logic gate that is part of a larger package.  It's not really clear from the manual how this is done and I find nothing useful on youtube in this area.  I have one symbol designed.  How do I go about making the part all together?

Thanks.

Rick

 

 

Simply add two times a symbol in the device, name it i.e. A and B and

use one package. Before I type a long letter here look at the

transistor-fet-lbr, device SI5902DC which might even suit you.

Check also for the add-level for each symbol.

 

--

Mit freundlichen Grüßen / With best regards

 

Joern Paschedag

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 14 years ago

    Am 27.01.2012 22:29, schrieb rickford66:

    Hi,

    I've created a dozen or so parts in libraries so far and, with a little help from the manual, youtube, and this forum, have had great success.  Now I'm trying to create a part with multiple "gates".  It's an 8 pin dual n-channel MOSFET.  I want the MOSFETs to be independent (A and B) like a regular logic gate that is part of a larger package.  It's not really clear from the manual how this is done and I find nothing useful on youtube in this area.  I have one symbol designed.  How do I go about making the part all together?

    Thanks.

    Rick

     

     

    Simply add two times a symbol in the device, name it i.e. A and B and

    use one package. Before I type a long letter here look at the

    transistor-fet-lbr, device SI5902DC which might even suit you.

    Check also for the add-level for each symbol.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag