Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) BC556 wrong pinout?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 189 subscribers
  • Views 773 views
  • Users 0 members are here
Related

BC556 wrong pinout?

Norfindel
Norfindel over 14 years ago

Hi. I just noticed that the pinout for the BC556B transistor seems to have collector and emitter reversed. It should be C - B - E looking at the printed (flat) side of the package with the pins going down.

 

Greetings.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    The only device I found was in the transistor.lbr as

    BC556B-PNP-TO92-EBC (*-PNP-)

    The only package currently associated was T092-EBC.  You need to add

    device to your library and then add the package TO92-CBE.

    ~Marvin

     

    On 1/29/2012 3:59 PM, Fernando Rapetti wrote:

    Hi i just noticed that the pinout for the BC556B transistor seems to have collector and emitter reversed. It should be C - B - E looking at the printed (flat) side of the package with the pins going down.

     

    Greetings.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Marvin Dawson schrieb:

     

    The only device I found was in the transistor.lbr as

    BC556B-PNP-TO92-EBC (*-PNP-)

    The only package currently associated was T092-EBC.  You need to add

    device to your library and then add the package TO92-CBE.

    ~Marvin

     

    On 1/29/2012 3:59 PM, Fernando Rapetti wrote:

    >> Hi i just noticed that the pinout for the BC556B transistor seems to have collector and emitter reversed. It should be C - B - E looking at the printed (flat) side of the package with the pins going down.

    >>

    >> Greetings.

     

    This is a perfect example of how to make it WRONG.

     

    Pads in packages should never get names according to their (real or

    intended) use. Pad names always are related to the physical package, not

    its content. In this case, the pad names of a TO-92 package are 1, 2 and

    3 (according to JEDEC). [This package can then be used for anything,

    like transistors, voltage regulators, diodes, varactors, thyristors, ID

    chips or whatever - remember that it's just the package.]

     

    The connection to the symbol (which has pin names B, C and E) is done in

    the device definition.

    If a part comes with different pinouts in the same package, it uses

    variants of the device with different connections - but not packages

    with differently named pads.

     

    The transistor.lbr ends up with about 10 image different TO-92 packages.

    Horrible.

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Norfindel
    Norfindel over 14 years ago in reply to e14 Contributor

    Thanks for the answers. I will add the device to my library, and make sure it uses a generic to-92 package.

    Is there a way to warn cadsoft about the misconfiguration on this transistor?

    I found this out after making the PCB. Fortunately, in this case i  can just turn the transistors around and not need to redo the PCB, it  could be much worse. Still, it was quite annoying.

    How is that the transistor library ended with so many packages? Can people upload their devices somehow, o just cadsoft did it that way?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Norfindel
    Norfindel over 14 years ago in reply to e14 Contributor

    Thanks for the answers. I will add the device to my library, and make sure it uses a generic to-92 package.

    Is there a way to warn cadsoft about the misconfiguration on this transistor?

    I found this out after making the PCB. Fortunately, in this case i  can just turn the transistors around and not need to redo the PCB, it  could be much worse. Still, it was quite annoying.

    How is that the transistor library ended with so many packages? Can people upload their devices somehow, o just cadsoft did it that way?