When parts are loaded from various Eagle libraries, the hole sizes in
through-hole parts can have all sorts of values. Some board
manufacturers charge extra if too many drill sizes are needed. It
seems it would be desirable to make some compromises on the hole sizes
to prevent, for instance, 0.039" holes and 0.040" holes in the same
design. Most likely these two sets of holes could be all one size.
Is there any built-in way in Eagle to accomplish this? I know I could
copy all the various parts from the Eagle libraries and make my own
custom versions of those parts for a given project in a special
project library. But that is a lot of work. Is there an easier way?
Robert Scott
Ypsilanti, Michigan