Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) invisible power pins on shematic
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 189 subscribers
  • Views 1105 views
  • Users 0 members are here
Related

invisible power pins on shematic

rickford66
rickford66 over 14 years ago

Hi,

Getting up to speed on Eagle.  Almost done with my first design.  Have a question about power pins.  On logic gates and such, the power pins are "invisible".  In order to connect them to the power and ground I desire, the only way I've found to do it is to bring the power pins into the schematic and connect them to the corresponding power and ground.  This leaves the pins visible on the schematic.  Doesn't that conflict with the idea that power pins are invisible? On my old DOS program, I made the pins visible, changed their attributes so they would connect to the appropriate net, then made them invisible again.  Can this be done in Eagle?

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    rickford66 wrote:

    Hi,

    Getting up to speed on Eagle. Almost done with my first design. Have

    a question about power pins. On logic gates and such, the power pins

    are "invisible". In order to connect them to the power and ground I

    desire, the only way I've found to do it is to bring the power pins

    into the schematic and connect them to the corresponding power and

    ground. This leaves the pins visible on the schematic. Doesn't that

    conflict with the idea that power pins are invisible? On my old DOS

    program, I made the pins visible, changed their attributes so they

    would connect to the appropriate net, then made them invisible again.

    Can this be done in Eagle? Thanks.

     

     

    Long story short. No.

    If you organise your libraries to have pin names that match the power rail

    names then the connections are automatic.

    If the logic libraries have a VCC pin then provide a VCC power supply. In

    this way  the power pins will connect automatically. If necessary give it a

    explanatory +5v label.

    If your libraries have a mix of power supply pin names then you will always

    have to manage the result.

    Power pins are not invisible in many instances. Often they are depicted in

    an area of the schematic with their associated decoupling capacitor.

     

    Warren

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Il 02/02/2012 21:33, Warren Brayshaw ha scritto:

     

    Long story short. No.

    If you organise your libraries to have pin names that match the power rail

    names then the connections are automatic.

    If the logic libraries have a VCC pin then provide a VCC power supply. In

    this way  the power pins will connect automatically. If necessary give it a

    explanatory +5v label.

    If your libraries have a mix of power supply pin names then you will always

    have to manage the result.

    Power pins are not invisible in many instances. Often they are depicted in

    an area of the schematic with their associated decoupling capacitor.

     

     

    I would add that the invisible pins should be avoided because it is very

    useful to know which pin is connected to the power supply, for debugging

    and test purposes.

     

    Marco

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Il 02/02/2012 21:33, Warren Brayshaw ha scritto:

     

    Long story short. No.

    If you organise your libraries to have pin names that match the power rail

    names then the connections are automatic.

    If the logic libraries have a VCC pin then provide a VCC power supply. In

    this way  the power pins will connect automatically. If necessary give it a

    explanatory +5v label.

    If your libraries have a mix of power supply pin names then you will always

    have to manage the result.

    Power pins are not invisible in many instances. Often they are depicted in

    an area of the schematic with their associated decoupling capacitor.

     

     

    I would add that the invisible pins should be avoided because it is very

    useful to know which pin is connected to the power supply, for debugging

    and test purposes.

     

    Marco