Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) invisible power pins on shematic
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 189 subscribers
  • Views 1104 views
  • Users 0 members are here
Related

invisible power pins on shematic

rickford66
rickford66 over 14 years ago

Hi,

Getting up to speed on Eagle.  Almost done with my first design.  Have a question about power pins.  On logic gates and such, the power pins are "invisible".  In order to connect them to the power and ground I desire, the only way I've found to do it is to bring the power pins into the schematic and connect them to the corresponding power and ground.  This leaves the pins visible on the schematic.  Doesn't that conflict with the idea that power pins are invisible? On my old DOS program, I made the pins visible, changed their attributes so they would connect to the appropriate net, then made them invisible again.  Can this be done in Eagle?

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    On Thu, 02 Feb 2012 18:57:46 +0000, rickford66 wrote:

     

    Hi,

    Getting up to speed on Eagle.  Almost done with my first design.  Have a

    question about power pins.  On logic gates and such, the power pins are

    "invisible".  In order to connect them to the power and ground I desire,

    the only way I've found to do it is to bring the power pins into the

    schematic and connect them to the corresponding power and ground.  This

    leaves the pins visible on the schematic.  Doesn't that conflict with

    the idea that power pins are invisible? On my old DOS program, I made

    the pins visible, changed their attributes so they would connect to the

    appropriate net, then made them invisible again.  Can this be done in

    Eagle? Thanks.

     

    Just an editorial comment:

     

    Over the years that I've been doing circuit design, I've developed a

    severe dislike for power pins that automagically connect up to specific

    nets.  First, because you have to have the right net names, and tools

    generally don't like you doing things like connecting "VCC" to "VDD". 

    Second, because as soon as you have more than one power net (e.g. a 3.3V

    digital and a 3.3V analog, or a 5V and a 3.3V VDD line, or a "regular" VDD

    and a "battery standby" VDD, etc.), then you need visible pins anyway. 

    Third, because you're never quite sure what net your power pins are

    supposed to be connected to, and so you have to do all this laborious

    checking.

     

    I, personally, and none of the engineering groups that I have worked in,

    have ever tolerated, much less preferred, the practices of hidden,

    automagically connecting, power pins.

     

    --

    My liberal friends think I'm a conservative kook.

    My conservative friends think I'm a liberal kook.

    Why am I not happy that they have found common ground?

     

    Tim Wescott, Communications, Control, Circuits & Software

    http://www.wescottdesign.com

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rickford66
    rickford66 over 14 years ago in reply to e14 Contributor

    I preferr visible pins too, but I don't want to re-do all the logic libraries.  When I design my own parts, they always have visible pins.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rickford66
    rickford66 over 14 years ago in reply to e14 Contributor

    I preferr visible pins too, but I don't want to re-do all the logic libraries.  When I design my own parts, they always have visible pins.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to rickford66

    Il 07/02/2012 15:27, rickford66 ha scritto:

     

    I preferr visible pins too, but I don't want to re-do all the logic libraries.  When I design my own parts, they always have visible pins.

     

     

    There's no need to change the libraries. Just invoke the power pins in

    the schematic.

     

    Marco

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to rickford66

    I thought it was just me being "behind the times" at my advanced age (61),

    glad to see others are not thrilled with "automagic pins" either.  Too bad

    there is not some option check box somewhere that says "show all hidden

    pins" or something.  I have always found that "intuitively obvious" will

    bite you !!  image

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.