Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) error message when replacing parts
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 190 subscribers
  • Views 859 views
  • Users 0 members are here
Related

error message when replacing parts

rickford66
rickford66 over 14 years ago

I have some parts on a sch/pcb that I need to replace with updated parts from the library.  I get the follow error message...

 

"Consistency lost during update!  No forward/backannotation will be performed!  Please contact CadSoft!"

 

followed by...

 

"The library update has failed!  Your drawing may be seriously damaged.  Please revert to a backup!"

 

I then close everything without saving, re-open and try again, but it keeps giving the same message.  Any ideas what's going on here?

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • robotonics
    robotonics over 14 years ago

    Yes, this is a really annoying problem. I usually have to delete the .brd file from the project and then allow the schematic to create a new board. Problem being that I lose time, especially if I have got the layout close to completion.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to robotonics

    On 2/3/2012 4:58 PM, David Cotterill-Drew wrote:

    Yes, this is a really annoying problem. I usually have to delete the .brd file from the project and then allow the schematic to create a new board. Problem being that I lose time, especially if I have got the layout close to completion.

     

     

    That's a bit overkill David,

     

    What's happening is that EAGLE replaces the component but doesn't

    reconnect the nets. Running the ERC will tell you where the consistency

    issues arise so that you can correct them manually, and that's a lot

    less work then starting the layout over generally.

     

    In some cases just moving the component and putting it back on the net

    connections takes care of the problem. Other times you can just add

    junction dots where the nets meet the part.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to robotonics

    On 2/3/2012 4:58 PM, David Cotterill-Drew wrote:

    Yes, this is a really annoying problem. I usually have to delete the .brd file from the project and then allow the schematic to create a new board. Problem being that I lose time, especially if I have got the layout close to completion.

     

     

    That's a bit overkill David,

     

    What's happening is that EAGLE replaces the component but doesn't

    reconnect the nets. Running the ERC will tell you where the consistency

    issues arise so that you can correct them manually, and that's a lot

    less work then starting the layout over generally.

     

    In some cases just moving the component and putting it back on the net

    connections takes care of the problem. Other times you can just add

    junction dots where the nets meet the part.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to rickford66

    On 2/8/2012 3:22 PM, rickford66 wrote:

    It seems that if I do a replace of a part that was originally from a different library it updates only the part being replaced.  If I replace a part with the same part from the same library, it updates all the parts by the same name in the schematic.  This seems to be when the error occurs, but it only occurs sometimes.  Also, to my surprise, when I update the part in the schematic, the corresponding part in the PCB is not updated to the latest in the library.  Is it supposed to work this way?

     

     

    Hi Rick,

     

    If the board and schematic are consistent then they both update, but if

    consistency is broken then they won't. Since the update bug causes a

    break in consistency this is a natural consequence.

     

    It's being worked on as we speak.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rickford66
    rickford66 over 14 years ago in reply to e14 Contributor

    It seems that if I do a replace of a part that was originally from a different library it updates only the part being replaced.  If I replace a part with the same part from the same library, it updates all the parts by the same name in the schematic.  This seems to be when the error occurs, but it only occurs sometimes.  Also, to my surprise, when I update the part in the schematic, the corresponding part in the PCB is not updated to the latest in the library.  Is it supposed to work this way?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to rickford66

    On 2/7/2012 11:14 AM, rickford66 wrote:

    When I did the replace, I found that the part, in this case, a polarized cap, was no longer connected.  Moving it away, then back reconnected it, but running electrical check again still shows same consistency errors.  "Different connections on C24 pin + and pad + (none / N$91)" and "Different connections on C24 pin - and pad - (none / AGND)  What does this mean?  Thanks.

     

     

    Hi Rick,

     

    Use the show command and click on the nets and make sure the pins light

    up, if they do then there should still be a connection.

     

    The alternative now would be to delete the offending signals on the

    board until consistency is restored, then hook everything up again. For

    the time being it may be better to avoid the replace command and simply

    delete and add the part again.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rickford66
    rickford66 over 14 years ago in reply to e14 Contributor

    When I did the replace, I found that the part, in this case, a polarized cap, was no longer connected.  Moving it away, then back reconnected it, but running electrical check again still shows same consistency errors.  "Different connections on C24 pin + and pad + (none / N$91)" and "Different connections on C24 pin - and pad - (none / AGND)  What does this mean?  Thanks.