Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Copy project UI problems and actual size suggestion
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 188 subscribers
  • Views 258 views
  • Users 0 members are here
Related

Copy project UI problems and actual size suggestion

e14 Contributor
e14 Contributor over 14 years ago

I just started using Eagle 6 and I think is awesome. I have two

suggestions that may not be too difficult to implement. They may already

been requested.

 

1 - I often need to copy a given project into the same directory as the

original under a new name. Generally this is to use an existing projects

as a sort of starting point for another.

There is a "copy" option in the context menu that shows up when right

clicking a folder in the control panel. This copy function gives me a

lot of, for me, useless options and restrictions, but does not allow me

to place the copy in the same directory as the original under a

different name. The suggested solution is allow it and to give the copy

a name such as "copy of xxxx" or allow to enter a new name.

Alternatively, the standard copy and paste functions, which are very

similar in Windows, Linux and Mac should be available.

 

 

2 - During the installation of Eagle, a step should be added to

calibrate Eagle to the screen pixel size of the monitor and video card

in use. This would happen only once unless the monitor or card are

replaced. After that, a command such as WINDOW ACTUALSIZE would zoom the

board or the package to the actual physical size of the board or

package, allowing to view the size of the design.

 

Thanks for considering these suggestions.

 

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Am 27.02.2012 16:19, schrieb George Blat:

    2 - During the installation of Eagle, a step should be added to

    calibrate Eagle to the screen pixel size of the monitor and video card

    in use. This would happen only once unless the monitor or card are

    replaced. After that, a command such as WINDOW ACTUALSIZE would zoom the

    board or the package to the actual physical size of the board or

    package, allowing to view the size of the design.

     

    Such an 'actual size' zoom would be quite useful - especially users not

    overly familiar with board design easily loose touch with reality on CAD

    software with nearly unlimited zoom possibilities. I see but two

    implementation problems with this:

      1. Putting it into the installation (and NOT letting the user change

         the settings later) could scare test users away. I myself would NOT

         want to go to the trouble of calibrating the screen for a software

         that I just wanted to play around with to see whether or not it's

         worth buying. Therefore:

          - DON'T put it in the installation, but somewhere in the main

            menu of the program.

          - DON'T ask the user for a screen calibration automatically.

          - Only IF the user tries WINDOW ACTUALSIZE, and the screen

            has NOT been calibrated so far, show the calibration dialog.

      2. In principle, horizontal and vertical sizes should be calibrated

         separately to allow for non-quadratic pixel sizes. Unfortunately,

         I doubt that EAGLE's screen drawing algorithm supports different

         scalings in X and Y direction. Changing the drawing algorithm

         accordingly is surely TOO much work, so the user should be content

         with an actual size zoom defined by ONE direction (the other

         could then be off on non-quadratic pixel monitors).

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    Am 27.02.2012 16:19, schrieb George Blat:

    2 - During the installation of Eagle, a step should be added to

    calibrate Eagle to the screen pixel size of the monitor and video card

    in use. This would happen only once unless the monitor or card are

    replaced. After that, a command such as WINDOW ACTUALSIZE would zoom the

    board or the package to the actual physical size of the board or

    package, allowing to view the size of the design.

     

    Such an 'actual size' zoom would be quite useful - especially users not

    overly familiar with board design easily loose touch with reality on CAD

    software with nearly unlimited zoom possibilities. I see but two

    implementation problems with this:

      1. Putting it into the installation (and NOT letting the user change

         the settings later) could scare test users away. I myself would NOT

         want to go to the trouble of calibrating the screen for a software

         that I just wanted to play around with to see whether or not it's

         worth buying. Therefore:

          - DON'T put it in the installation, but somewhere in the main

            menu of the program.

          - DON'T ask the user for a screen calibration automatically.

          - Only IF the user tries WINDOW ACTUALSIZE, and the screen

            has NOT been calibrated so far, show the calibration dialog.

      2. In principle, horizontal and vertical sizes should be calibrated

         separately to allow for non-quadratic pixel sizes. Unfortunately,

         I doubt that EAGLE's screen drawing algorithm supports different

         scalings in X and Y direction. Changing the drawing algorithm

         accordingly is surely TOO much work, so the user should be content

         with an actual size zoom defined by ONE direction (the other

         could then be off on non-quadratic pixel monitors).

     

    Andreas Weidner