Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle and the libpng situation
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 189 subscribers
  • Views 1147 views
  • Users 0 members are here
Related

Eagle and the libpng situation

e14 Contributor
e14 Contributor over 14 years ago

I know this is an old issue and people have done work arounds, but building against libpng14 did create a lot of problems for linux users whose distros do not have libpng14 (something like 4 out of the top 5 distros, and 7 out of the top 10 don't have it). It appears now that they will never have libpng14. In fact, libpng's own website encourages the use of 12 or 15...

 

Could CadSoft either:

1) build against libpng15, if possible

2) include libpng.so.14 with the release or statically link against libpng14

 

CadSoft has said that (2) is impossible for legal reasons, but that doesn't make sense. libpng's license is:

 

" Permission is hereby granted to use, copy, modify, and distribute this

  source code, or portions hereof, for any purpose, without fee, subject

  to the following restrictions:

 

  1. The origin of this source code must not be misrepresented.

 

  2. Altered versions must be plainly marked as such and

     must not be misrepresented as being the original source.

 

  3. This Copyright notice may not be removed or altered from

     any source or altered source distribution.

 

  The Contributing Authors and Group 42, Inc. specifically permit, without

  fee, and encourage the use of this source code as a component to

  supporting the PNG file format in commercial products.  If you use this

  source code in a product, acknowledgment is not required but would be

  appreciated."

 

Which allows, with no preconditions, CadSoft to include libpng14 with their binary for eagle. It explicitly says you can use it in commerical products and doesn't even require you to acknowledge that you did (although I would encourage you to). It's an extremely generous license which in fact allows you to even statically compile the library into eagle and distribute the binary that way (with the proper attribution in your readme or license file). However, that may be a security threat and thus a liabillity.

 

If you're worried about security, then you can do (1) and rely on distributions to keep the library up to date to reduce your liabillity.

 

Thanks for your consideration, and hopefully this is something that can be easily worked out.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    I just saw the changelog of version 6.2.1:

      - Linux: libpng and libjpeg directly linked into the executable to get rid of

        dependency and availability of according system libs.

     

    Thanks! That's a great move, we appreciate it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    I just saw the changelog of version 6.2.1:

      - Linux: libpng and libjpeg directly linked into the executable to get rid of

        dependency and availability of according system libs.

     

    Thanks! That's a great move, we appreciate it.