I have a library (lib file) that I am adding parts to. It was
originally created under Eagle 5.
I added a new IC to this library file, during a trip, using Eagle 6.1.0
Professional on a laptop running Windows 7 32 bit.
Now, when back at work, I copy the library file to my desktop computer
running Eagle 6.1.0 or 6.2.0 Professional, the new I.C. is not visible,
but all the older parts are still there in the library. The desktop
computer is running Windows 7, 64 bit.
When I look in 6.1.0 on the laptop, in the same file, the new part is
there. When I look in 6.1.0 or 6.2.0 on the desktop computer, the new
part is not there.
This is a large IC, that took several hours to create the footprint,
symbol, part, etc.
I have already spent several hours more going back and forth from the
laptop to the desktop to make sure that I have the correct version of
the file, and copying several times, to the lib file inside of the
Program files folder as well as trying to put it in the lib file in
the %appdata% folder.
How do I get my new part to be usable on my desktop Windows 7 64 computer?
--- Graham
==