Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) How to Change 0,0 point in grid?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 189 subscribers
  • Views 1459 views
  • Users 0 members are here
Related

How to Change 0,0 point in grid?

e14 Contributor
e14 Contributor over 14 years ago

Hello, I often find myself needing to change the zero point in the

layout grid. For example, I develop board, then I change size or shape,

for example, I add rails to the PCB or something, and I want to change

the 0,0 point so that the new board shape and size is correctly placed

within the grid. Is there a way to do this without having to copy the

entire design and manually move that entire selection, aligning it by

eye to the 0,0 marking?

 

Thanx,

 

Tony

 

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    tony wrote:

     

    >On 4/26/12 4:24 PM, Andrew Sterian wrote:

    >> On 4/26/12 2:49 PM, tony wrote:

    >>> Hello, I often find myself needing to change the zero point in the

    >>> layout grid. For example, I develop board, then I change size or shape,

    >>> for example, I add rails to the PCB or something, and I want to change

    >>> the 0,0 point so that the new board shape and size is correctly placed

    >>> within the grid.

    >[...] Many times I forget about parts that are locked, or I

    >forget to turn on all layers or something, and I really whack things!

     

    if you don't need the parts relocked after move you could expand on

    Chucks command sequence by inserting

     

      lock (CS> 0 0)

     

    between "group all" and "move ..."

     

     

    You could also use the mark command to indicate the new origin.

    In that case the move command does not need to deal with absolute

    coordinates at all, so you can put the commands in a script file.

     

      move (R> 0 0) (0 0)

     

    (see "Editor Commands - Command Syntax" in the online help for an

    explanation of the modifiers)

     

     

    If you want the locks preserved, you will need to write an ULP that

    records the names of the locked parts and puts the lock in place again

    after the move.

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 14 years ago in reply to e14 Contributor

    On 04/26/2012 04:24 PM, Andrew Sterian wrote:

    On 4/26/12 2:49 PM, tony wrote:

    >> Hello, I often find myself needing to change the zero point in the

    >> layout grid.

    ...

    >> Thanx,

    >>

    >> Tony

     

    There's no easy way to change the 0,0 point as far as I know. You could

    always use the "mark" command to set a relative 0,0 point, but that's

    not a particularly good solution.

     

    What I do is:

     

    • Figure out where the lower-left origin of your design actually is (say

    (0.15",0.25") for example)

     

    You can do it from the command line without messing with the grid.

    From the eagle command line:

     

         display all;

         group all;

         move (>0.15 0.25) (0 0);

         display last;

     

    The ">" in the move command is equivalent to a Ctrl-LeftClick, which

    would grab the entire group at the desired origin.

     

    Since the desired origin is not always in the same place, it doesn't

    make much sense to put this into a .scr file.

     

    Hope this helps,

        - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 4/26/12 4:24 PM, Andrew Sterian wrote:

    On 4/26/12 2:49 PM, tony wrote:

    >> Hello, I often find myself needing to change the zero point in the

    >> layout grid. For example, I develop board, then I change size or shape,

    >> for example, I add rails to the PCB or something, and I want to change

    >> the 0,0 point so that the new board shape and size is correctly placed

    >> within the grid. Is there a way to do this without having to copy the

    >> entire design and manually move that entire selection, aligning it by

    >> eye to the 0,0 marking?

    >>

    >> Thanx,

    >>

    >> Tony

     

    There's no easy way to change the 0,0 point as far as I know. You could

    always use the "mark" command to set a relative 0,0 point, but that's

    not a particularly good solution.

     

    What I do is:

     

    • Figure out where the lower-left origin of your design actually is (say

    (0.15",0.25") for example)

    • Type 'disp all' to display everything (and make sure nothing is locked

    down)

    • Group everything

    • Type "grid 0.15" to prepare to move everything to the left

    • Move the group to the left by one mouse jog, which will be 0.15"

    because of the grid

    • Repeat the process by setting the grid to 0.25" then move the group

    down, which should then land on the origin.

     

    If there's a ULP that does the above, I'd love to know!

     

    Andrew.

     

    Thanx for the response.

     

    Yeah that is similar to what I am doing. I just dis-like moving things

    around like that. Many times I forget about parts that are locked, or I

    forget to turn on all layers or something, and I really whack things!

     

    A way to just change the 0,0 Mark would be excellent.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    On 4/26/12 2:49 PM, tony wrote:

    Hello, I often find myself needing to change the zero point in the

    layout grid. For example, I develop board, then I change size or shape,

    for example, I add rails to the PCB or something, and I want to change

    the 0,0 point so that the new board shape and size is correctly placed

    within the grid. Is there a way to do this without having to copy the

    entire design and manually move that entire selection, aligning it by

    eye to the 0,0 marking?

     

    Thanx,

     

    Tony

     

    There's no easy way to change the 0,0 point as far as I know. You could

    always use the "mark" command to set a relative 0,0 point, but that's

    not a particularly good solution.

     

    What I do is:

     

    • Figure out where the lower-left origin of your design actually is (say

    (0.15",0.25") for example)

    • Type 'disp all' to display everything (and make sure nothing is locked

    down)

    • Group everything

    • Type "grid 0.15" to prepare to move everything to the left

    • Move the group to the left by one mouse jog, which will be 0.15"

    because of the grid

    • Repeat the process by setting the grid to 0.25" then move the group

    down, which should then land on the origin.

     

    If there's a ULP that does the above, I'd love to know!

     

    Andrew.