Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) pick and place file
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 188 subscribers
  • Views 1021 views
  • Users 0 members are here
Related

pick and place file

e14 Contributor
e14 Contributor over 14 years ago

I need to generate a pick and place file for automatic assembly with the following fields :

part ref / value / package / orientation / position  X Y.

I need the value of the component (for instance : 4,7K, 10uF, Pic16f877...), but the file generated by running "smdmount.ulp" does not give this field.

The file generated by "export partlist" gives everything that is needed, but not the side (top or bottom).

How can I do ?

  • Sign in to reply
  • Cancel
  • dukepro
    dukepro over 14 years ago

    On 04/29/2012 10:22 AM, jerome sejournet wrote:

    I need to generate a pick and place file for automatic assembly with

    the following fields : part ref / value / package / orientation /

    position  X Y. I need the value of the component (for instance :

    4,7K, 10uF, Pic16f877...), but the file generated by running

    "smdmount.ulp" does not give this field. The file generated by

    "export partlist" gives everything that is needed, but not the side

    (top or bottom). How can I do ?

     

     

    Jerome,

     

    Try playing with the attached ULP.  It doesn't have the part value in

    it, but you could add that in the same manner that partName[] or

    partPackage[] is handled.  I think I pulled this from some other script,

    then bastardized it to suite my needs.

     

    It presents the user with an on-screen list with an option to save to a

    CSV file.

     

    Hope this helps.

     

        - Chuck

     

    Attachments:
    origins.ulp.zip