Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Unable to re-locate ULP directory
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 189 subscribers
  • Views 488 views
  • Users 0 members are here
Related

Unable to re-locate ULP directory

bvwj
bvwj over 14 years ago

When I move the ULP directory to a user direcory (running OSX) I get a fatal error every time I launch a ulp from the command input box.  "run bom.ulp" generates a "unknown identifier 'book'" error box then locks up the entire Eagle application.  At that point I have to force quit Eagle.  I moved the ULP directory back and it works again, but it would be nice to have the ULP directory away from the read only applications directory where it gets installed.

 

I can run ULPs in the alternate directory through the menu selection and file dialog process without the error, but the command input box is preferred.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Barry Walker wrote:

    >When I move the ULP directory to a user direcory (running OSX) I get a fatal error every time

    >I launch a ulp from the command input box.  "run bom.ulp" generates a "unknown identifier

    'book'" error box then locks up the entire Eagle application.  At that point I have to force quit

    Eagle. 

     

    have changed the 'User Language Programs' path in

    'Control Panel - Options - Directories' accordingly?

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bvwj
    bvwj over 14 years ago in reply to e14 Contributor

    Yes, I tried changing it to a few different locations and the error always occurs unless the default directory is used.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bvwj
    bvwj over 14 years ago in reply to e14 Contributor

    Yes, I tried changing it to a few different locations and the error always occurs unless the default directory is used.