Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Project-specific configs - esp. drills, dimension
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 336 views
  • Users 0 members are here
Related

Project-specific configs - esp. drills, dimension

e14 Contributor
e14 Contributor over 14 years ago

One thing that is quite bothersome is how the various parameters configurable under the Options->Set menu are handled.  It would really make sense for some of those parameters to be project-specific, the Drills in particular.  The drill table changes across projects so, when used in conjunction with the drillegend-stack ULP (which requires the drills to be sorted by size), universally changing the drill table gets cumbersome.  This is particularly onerous when switching between multiple projects, which I do frequently.  Placing the drill table within the auspices of individual projects will keep them proper.

 

One other related suggestion would be a Sort button in the drill table dialog.  I use drillegend-stack ULP to generate the drill table for my fabricator.  Having to go in a manually sort the drill table is a manual task that should be readily automated.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

     

    "Eric Deuel" <noreply-62020@element14.com> a écrit dans le message de news:

    1009267270.10811336500410255.JavaMail.jive@flcspu-csapp-01.premierfarnell.com...

    One thing that is quite bothersome is how the various parameters configurable under the

    Options->Set menu are handled. It would really make sense for some of those parameters to be

    project-specific,

     

    You said "PROJECT oriented" ? see this topic:

    http://www.eaglecentral.ca/forums/index.php?t=msg&th=46900&start=0&546e8117397602c11c874278d866e33a/

     

    the Drills in particular. The drill table changes across projects so, when used in conjunction with

    the drillegend-stack ULP (which requires the drills to be sorted by size), universally changing the

    drill table gets cumbersome. This is particularly onerous when switching between multiple projects,

    which I do frequently. Placing the drill table within the auspices of individual projects will keep

    them proper.

     

    The drill table is saved in the "eaglerc.usr" file. This is one of the reasons why I have to copy

    this file in each of my project-directories.

    I think that the drill table is specific for each board and should be saved in the board (as for

    the DRC parameters).

     

    One other related suggestion would be a Sort button in the drill table dialog.

     

    This is a very old old old request :o(((

    We could easily do that with an ULP but unfortunately the drill.symbol parameters as:

    SET Drill.Symbol.Nr.4 = 0.8mm; doesn't works in the command line.

     

    I use drillegend-stack ULP to generate the drill table for my fabricator. Having to go in a

    manually sort the drill table is a manual task that should be readily automated.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

     

    "Eric Deuel" <noreply-62020@element14.com> a écrit dans le message de news:

    1009267270.10811336500410255.JavaMail.jive@flcspu-csapp-01.premierfarnell.com...

    One thing that is quite bothersome is how the various parameters configurable under the

    Options->Set menu are handled. It would really make sense for some of those parameters to be

    project-specific,

     

    You said "PROJECT oriented" ? see this topic:

    http://www.eaglecentral.ca/forums/index.php?t=msg&th=46900&start=0&546e8117397602c11c874278d866e33a/

     

    the Drills in particular. The drill table changes across projects so, when used in conjunction with

    the drillegend-stack ULP (which requires the drills to be sorted by size), universally changing the

    drill table gets cumbersome. This is particularly onerous when switching between multiple projects,

    which I do frequently. Placing the drill table within the auspices of individual projects will keep

    them proper.

     

    The drill table is saved in the "eaglerc.usr" file. This is one of the reasons why I have to copy

    this file in each of my project-directories.

    I think that the drill table is specific for each board and should be saved in the board (as for

    the DRC parameters).

     

    One other related suggestion would be a Sort button in the drill table dialog.

     

    This is a very old old old request :o(((

    We could easily do that with an ULP but unfortunately the drill.symbol parameters as:

    SET Drill.Symbol.Nr.4 = 0.8mm; doesn't works in the command line.

     

    I use drillegend-stack ULP to generate the drill table for my fabricator. Having to go in a

    manually sort the drill table is a manual task that should be readily automated.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Thanks for the insight.  After reading and implementing your suggestions from the linked topic, I discovered changing my HOME variable did bad things to other apps so had to change that back.  I've spent a bit more time looking at the various forum threads on the eaglerc.usr file and ran across the -U switch added to the command line options after Eagle v5.11.  Now my shortcut command line reads something like "eagle.exe -U.\eaglerc.usr" which points to the file local to the shortcut.  It is a bit of an annoyance to have to navigate to the project folder to launch Eagle rather than the pinned shortcut but it is a small price to pay.  I sincerely hope that this becomes easier in succeeding revisions - like defaulting to the .usr file in the project file if it exists before going to a global location like HOME.  Just a thought.