Hi All,
I'm new to Eagle and I must say I'm impressed by the ease of use and the
level of documentation and support.
I'm currently working on a PCB that connects to an existing board with
right angle IDC connectors. The existing board offers a 30pins IDC header
therefore the board I'm designing needs a 30pins IDC socket.
Unfortunately, I've been unable to find such socket in the library
provided, only the header (PAK100/2500-5-30 in con-3m.lbr). I've installed
the default libs that come with Eagle 6.2.0 for Windows.
Can anyone guide me to a lib containing this component, if it exists? I've
attached a pic as an example (14 pins only though).
Thanks,
George
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.