Hello,
Is there a way to set the default drill and diameter for vias ? I mean the values on the toolbar drop down box when you are routing wires, they will keep to reset to auto and 0.27...something. when the program is restarted. this is very annoying.
It would be nice to have a way to keep other settings like the line angle style (I want 45 degree angles and it keeps to reset to 90 degree angles...).
Regards.