Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Bug? Library part pins silently autoconnected to matching schematic net names
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 188 subscribers
  • Views 1510 views
  • Users 0 members are here
Related

Bug? Library part pins silently autoconnected to matching schematic net names

e14 Contributor
e14 Contributor over 14 years ago

Hi,

Ran into this strange and potentially dangerous behavior today in EAGLE 6.0.0 / 6.2.0. If a pin in a library symbol has direction 'Pwr' (possibly others?), if a net with the same name exists in the schematic, the pin is being automatically and silently connected in the Board editor (no visible connection or other indication of this being the case in the Schematic editor). No questions asked, no warnings, no way to 'undo' (except by deleting the offending part / rolling back to a point before the part was introduced, renaming the net, and re-importing the part). If this has occurred, connecting the actually intended net (if any) to the pin in the Schematic editor results in shorting the nets together in the Board editor.

 

The fact that only certain pins (notably 'Pwr') are affected suggests this dangerous behavior may be intentional. Is there any way to a) disable this behavior, b) generate a loud warning whenever it is triggered, and/or c) undo the behavior when it is triggered?

 

Some specific objections to this being a default behavior:

  • Many library part authors (really, many part manufacturers, who library part authors dutifully copy) use power pin names such as Vin/Vcc/Vdd/V+ somewhat interchangeably; these names do not uniquely refer to any voltage standard
  • Many schematic authors (including more than one at my day-job) sometimes use the default names for the 'supply' symbols to designate different power nets on mixed-voltage boards (e.g. the 'Vcc' symbol for 5V and 'Vdd' symbol for 3.3V), wreaking havoc with the previous case. You would never know your part is being overvolted by this behavior (silently connected to wrong supply), or your supply nets are shorted together, without careful visual inspection of the ratsnest lines.
  • Likewise for ground splitting - I presume (but have not yet tested) a Pwr pin named 'GND' will exhibit the same behavior, causing a problem where e.g. a specific part of the circuit requires a split ground (e.g. AGND), where elsewhere in the design, a library part that does not need, and should not use the elsewhere AGND offers GND/AGND pins. GND/AGND will then be shorted together at the 2nd location.
  • Nets connected in the Board / design but explicitly shown as unconnected in the schematic - this should never happen!
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Tim Gipson wrote on Tue, 19 June 2012 10:50

    Hi,

    Ran into this strange and potentially dangerous behavior today in EAGLE

    6.0.0 / 6.2.0. If a pin in a library symbol has direction 'Pwr' (possibly

    others?), if a net with the same name exists in the schematic, the pin is

    being automatically and silently connected in the Board editor (no

    visible connection or other indication of this being the case in the

    Schematic editor). No questions asked, no warnings, no way to 'undo'

    (except by deleting the offending part / rolling back to a point before

    the part was introduced, renaming the net, and re-importing the part). If

    this has occurred, connecting the actually intended net (if any) to the

    pin in the Schematic editor results in shorting the nets together in the

    Board editor.

     

    The fact that only certain pins (notably 'Pwr') are affected suggests

    this dangerous behavior may be intentional. Is there any way to a)

    disable this behavior, b) generate a loud warning whenever it is

    triggered, and/or c) undo the behavior when it is triggered?

     

    Some specific objections to this being a default behavior:

    • Many library part authors (really, many part manufacturers, who

    library part authors dutifully copy) use power pin names such as

    Vin/Vcc/Vdd/V+ somewhat interchangeably; these names do not uniquely

    refer to any voltage standard

    • Many schematic authors (including more than one at my day-job)

    sometimes use the default names for the 'supply' symbols to designate

    different power nets on mixed-voltage boards (e.g. the 'Vcc' symbol for

    5V and 'Vdd' symbol for 3.3V), wreaking havoc with the previous case. You

    would never know your part is being overvolted by this behavior (silently

    connected to wrong supply), or your supply nets are shorted together,

    without careful visual inspection of the ratsnest lines.

    • Likewise for ground splitting - I presume (but have not yet tested) a

    Pwr pin named 'GND' will exhibit the same behavior, causing a problem

    where e.g. a specific part of the circuit requires a split ground (e.g.

    AGND), where elsewhere in the design, a library part that does not need,

    and should not use the elsewhere AGND offers GND/AGND pins. GND/AGND will

    then be shorted together at the 2nd location.

    • Nets connected in the Board / design but explicitly shown as

    unconnected in the schematic - this should never happen!

     

     

    Hello Tim,

     

    This is not a bug, it's a feature!  I know you've heard that before but

    this is actually intended.  Now I agree with you that nothing should ever

    be connected in the PCB that isn't explicitly drawn on the schematic.  But

    this is how EAGLE does it.

     

    From the help for the "PIN" command:

     

    Quote:

    If Pwr pins are used on a symbol and a corresponding Sup pin exists on

    the schematic, nets are connected automatically.

     

     

    My solution is to never, ever, use parts without invoking all gates on all

    parts.  At least then all the pins are visible.

     

    I would like to see a switch to disable this behaviour.  Perhaps an entry

    for the SET command.  CadSoft?

     

    Cheers,

     

    James.

    --

    James Morrison  ~~~  Stratford Digital

     

    Specializing in CadSoft EAGLE

    • Online Sales to North America

    • Electronic Design Services

    • EAGLE Enterprise Toolkit

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 19.06.2012 17:13, James Morrison wrote:

    Tim Gipson wrote on Tue, 19 June 2012 10:50

    >> Hi,

    >> Ran into this strange and potentially dangerous behavior today in EAGLE

    >> 6.0.0 / 6.2.0. If a pin in a library symbol has direction 'Pwr' (possibly

    >> others?), if a net with the same name exists in the schematic, the pin is

    >> being automatically and silently connected in the Board editor (no

    >> visible connection or other indication of this being the case in the

    >> Schematic editor). No questions asked, no warnings, no way to 'undo'

    >> (except by deleting the offending part / rolling back to a point before

    >> the part was introduced, renaming the net, and re-importing the part). If

    >> this has occurred, connecting the actually intended net (if any) to the

    >> pin in the Schematic editor results in shorting the nets together in the

    >> Board editor.

    >>

    >> The fact that only certain pins (notably 'Pwr') are affected suggests

    >> this dangerous behavior may be intentional. Is there any way to a)

    >> disable this behavior, b) generate a loud warning whenever it is

    >> triggered, and/or c) undo the behavior when it is triggered?

    >>

    >> Some specific objections to this being a default behavior:

    >> * Many library part authors (really, many part manufacturers, who

    >> library part authors dutifully copy) use power pin names such as

    >> Vin/Vcc/Vdd/V+ somewhat interchangeably; these names do not uniquely

    >> refer to any voltage standard

    >> * Many schematic authors (including more than one at my day-job)

    >> sometimes use the default names for the 'supply' symbols to designate

    >> different power nets on mixed-voltage boards (e.g. the 'Vcc' symbol for

    >> 5V and 'Vdd' symbol for 3.3V), wreaking havoc with the previous case. You

    >> would never know your part is being overvolted by this behavior (silently

    >> connected to wrong supply), or your supply nets are shorted together,

    >> without careful visual inspection of the ratsnest lines.

    >> * Likewise for ground splitting - I presume (but have not yet tested) a

    >> Pwr pin named 'GND' will exhibit the same behavior, causing a problem

    >> where e.g. a specific part of the circuit requires a split ground (e.g.

    >> AGND), where elsewhere in the design, a library part that does not need,

    >> and should not use the elsewhere AGND offers GND/AGND pins. GND/AGND will

    >> then be shorted together at the 2nd location.

    >> * Nets connected in the Board / design but explicitly shown as

    >> unconnected in the schematic - this should never happen!

    >

    Hello Tim,

     

    This is not a bug, it's a feature!  I know you've heard that before but

    this is actually intended.  Now I agree with you that nothing should ever

    be connected in the PCB that isn't explicitly drawn on the schematic.  But

    this is how EAGLE does it.

     

    From the help for the "PIN" command:

     

    Quote:

    >> If Pwr pins are used on a symbol and a corresponding Sup pin exists on

    >> the schematic, nets are connected automatically.

    >

    My solution is to never, ever, use parts without invoking all gates on all

    parts.  At least then all the pins are visible.

     

    I would like to see a switch to disable this behaviour.  Perhaps an entry

    for the SET command.  CadSoft?

     

    Cheers,

     

    James.

     

     

    Hello Tim, James,

     

    EAGLE connects Pwr pins with same names automatically, that's true.

    Even not invoked Pwr pins will be connected.

    To have this all under control EAGLE runs several checks (ERC).

    For each Pwr signal in the schematic EAGLE wants you to place a

    supply pin on every sheet.

    ERC message: "No supply for power pin xxxxx" helps in identifying

    pwr signals. And there are additional checks on Pwr signals.

    That's the way EAGLE works for about 20 years now......

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    CadSoft Support wrote on Wed, 20 June 2012 03:02

    EAGLE connects Pwr pins with same names automatically, that's true.

    Even not invoked Pwr pins will be connected.

    To have this all under control EAGLE runs several checks (ERC).

    For each Pwr signal in the schematic EAGLE wants you to place a

    supply pin on every sheet.

    ERC message: "No supply for power pin xxxxx" helps in identifying

    pwr signals. And there are additional checks on Pwr signals.

    That's the way EAGLE works for about 20 years now......

     

     

    I understand all of that Richard.  But electronics have evolved a bit in 20

    years--maybe EAGLE should too!  20 years ago you might have had an entire

    board powered by 5V so one rail called VCC was very useful.  Most boards I

    do today have 5+ different power voltages so this is no longer the case.

     

    And having connections done in the PCB that aren't shown in the schematic

    is VERY BAD PRACTICE.  When I'm debugging a board I need to be able to tell

    all of the exact connections.  The possibility of implicit and hidden

    connections is enough for some companies to not even consider EAGLE since

    it breaks internal design process requirements.  Having a SET command that

    could turn this off would be a great compromise.

     

    James.

    --

    James Morrison  ~~~  Stratford Digital

     

    Specializing in CadSoft EAGLE

    • Online Sales to North America

    • Electronic Design Services

    • EAGLE Enterprise Toolkit

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    I just wanted to illustrate the havoc it causes me.. This is just a tiny

    part of my very long ERC list (8  pages long, and I have 1600 pixel high

    screen). At least it could have merged alot of these warnings into one.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Count me in! Again!

    This stuff only makes my ERC more painful.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    James Morrison wrote on Wed, 20 June 2012 11:37

    And having connections done in the PCB that aren't shown in the

    schematic is VERY BAD PRACTICE.  When I'm debugging a board I need to be

    able to tell all of the exact connections.  The possibility of implicit

    and hidden connections is enough for some companies to not even consider

    EAGLE since it breaks internal design process requirements.  Having a SET

    command that could turn this off would be a great compromise.

     

     

    I totally agree.  It's really about time Cadsoft fixes this.  This has been

    brought up by many people many times before.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 21.06.2012 07:24, schrieb Lorenz:

    Andrew Sterian wrote:

    >> On 6/20/12 11:37 AM, James Morrison wrote:

    >>> CadSoft Support wrote on Wed, 20 June 2012 03:02

    >>>> EAGLE connects Pwr pins with same names automatically, that's true.

    >>>> Even not invoked Pwr pins will be connected.

    >>

    >> Please do update EAGLE's approach for 2012: recognize that boards have

    >> multiple voltages, there is no such thing as "VCC" anymore, and NOTHING

    >> should be connected that is not visible on the schematic.

     

    as it is best practice to create you own libraries, just don't use PWR

    pins (only on power symbols).

     

     

    I agree with Lorenz in creating/modifying my own libraries. I also use

    the same names given in the data sheets incl. VDD,VSS etc. BUT I don't

    use these names as supply in drawings and so there is no automatic

    connection. And even if there is a fancy supply voltage like 2.347861

    then there will be a new supply connected to the device VCC. I get a

    warning and that is OK and accepted.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 21.06.2012 07:24, schrieb Lorenz:

    Andrew Sterian wrote:

    >> On 6/20/12 11:37 AM, James Morrison wrote:

    >>> CadSoft Support wrote on Wed, 20 June 2012 03:02

    >>>> EAGLE connects Pwr pins with same names automatically, that's true.

    >>>> Even not invoked Pwr pins will be connected.

    >>

    >> Please do update EAGLE's approach for 2012: recognize that boards have

    >> multiple voltages, there is no such thing as "VCC" anymore, and NOTHING

    >> should be connected that is not visible on the schematic.

     

    as it is best practice to create you own libraries, just don't use PWR

    pins (only on power symbols).

     

     

    I agree with Lorenz in creating/modifying my own libraries. I also use

    the same names given in the data sheets incl. VDD,VSS etc. BUT I don't

    use these names as supply in drawings and so there is no automatic

    connection. And even if there is a fancy supply voltage like 2.347861

    then there will be a new supply connected to the device VCC. I get a

    warning and that is OK and accepted.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag