Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Bug? Library part pins silently autoconnected to matching schematic net names
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 188 subscribers
  • Views 1507 views
  • Users 0 members are here
Related

Bug? Library part pins silently autoconnected to matching schematic net names

e14 Contributor
e14 Contributor over 14 years ago

Hi,

Ran into this strange and potentially dangerous behavior today in EAGLE 6.0.0 / 6.2.0. If a pin in a library symbol has direction 'Pwr' (possibly others?), if a net with the same name exists in the schematic, the pin is being automatically and silently connected in the Board editor (no visible connection or other indication of this being the case in the Schematic editor). No questions asked, no warnings, no way to 'undo' (except by deleting the offending part / rolling back to a point before the part was introduced, renaming the net, and re-importing the part). If this has occurred, connecting the actually intended net (if any) to the pin in the Schematic editor results in shorting the nets together in the Board editor.

 

The fact that only certain pins (notably 'Pwr') are affected suggests this dangerous behavior may be intentional. Is there any way to a) disable this behavior, b) generate a loud warning whenever it is triggered, and/or c) undo the behavior when it is triggered?

 

Some specific objections to this being a default behavior:

  • Many library part authors (really, many part manufacturers, who library part authors dutifully copy) use power pin names such as Vin/Vcc/Vdd/V+ somewhat interchangeably; these names do not uniquely refer to any voltage standard
  • Many schematic authors (including more than one at my day-job) sometimes use the default names for the 'supply' symbols to designate different power nets on mixed-voltage boards (e.g. the 'Vcc' symbol for 5V and 'Vdd' symbol for 3.3V), wreaking havoc with the previous case. You would never know your part is being overvolted by this behavior (silently connected to wrong supply), or your supply nets are shorted together, without careful visual inspection of the ratsnest lines.
  • Likewise for ground splitting - I presume (but have not yet tested) a Pwr pin named 'GND' will exhibit the same behavior, causing a problem where e.g. a specific part of the circuit requires a split ground (e.g. AGND), where elsewhere in the design, a library part that does not need, and should not use the elsewhere AGND offers GND/AGND pins. GND/AGND will then be shorted together at the 2nd location.
  • Nets connected in the Board / design but explicitly shown as unconnected in the schematic - this should never happen!
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Tim Gipson wrote on Tue, 19 June 2012 10:50

    Hi,

    Ran into this strange and potentially dangerous behavior today in EAGLE

    6.0.0 / 6.2.0. If a pin in a library symbol has direction 'Pwr' (possibly

    others?), if a net with the same name exists in the schematic, the pin is

    being automatically and silently connected in the Board editor (no

    visible connection or other indication of this being the case in the

    Schematic editor). No questions asked, no warnings, no way to 'undo'

    (except by deleting the offending part / rolling back to a point before

    the part was introduced, renaming the net, and re-importing the part). If

    this has occurred, connecting the actually intended net (if any) to the

    pin in the Schematic editor results in shorting the nets together in the

    Board editor.

     

    The fact that only certain pins (notably 'Pwr') are affected suggests

    this dangerous behavior may be intentional. Is there any way to a)

    disable this behavior, b) generate a loud warning whenever it is

    triggered, and/or c) undo the behavior when it is triggered?

     

    Some specific objections to this being a default behavior:

    • Many library part authors (really, many part manufacturers, who

    library part authors dutifully copy) use power pin names such as

    Vin/Vcc/Vdd/V+ somewhat interchangeably; these names do not uniquely

    refer to any voltage standard

    • Many schematic authors (including more than one at my day-job)

    sometimes use the default names for the 'supply' symbols to designate

    different power nets on mixed-voltage boards (e.g. the 'Vcc' symbol for

    5V and 'Vdd' symbol for 3.3V), wreaking havoc with the previous case. You

    would never know your part is being overvolted by this behavior (silently

    connected to wrong supply), or your supply nets are shorted together,

    without careful visual inspection of the ratsnest lines.

    • Likewise for ground splitting - I presume (but have not yet tested) a

    Pwr pin named 'GND' will exhibit the same behavior, causing a problem

    where e.g. a specific part of the circuit requires a split ground (e.g.

    AGND), where elsewhere in the design, a library part that does not need,

    and should not use the elsewhere AGND offers GND/AGND pins. GND/AGND will

    then be shorted together at the 2nd location.

    • Nets connected in the Board / design but explicitly shown as

    unconnected in the schematic - this should never happen!

     

     

    Hello Tim,

     

    This is not a bug, it's a feature!  I know you've heard that before but

    this is actually intended.  Now I agree with you that nothing should ever

    be connected in the PCB that isn't explicitly drawn on the schematic.  But

    this is how EAGLE does it.

     

    From the help for the "PIN" command:

     

    Quote:

    If Pwr pins are used on a symbol and a corresponding Sup pin exists on

    the schematic, nets are connected automatically.

     

     

    My solution is to never, ever, use parts without invoking all gates on all

    parts.  At least then all the pins are visible.

     

    I would like to see a switch to disable this behaviour.  Perhaps an entry

    for the SET command.  CadSoft?

     

    Cheers,

     

    James.

    --

    James Morrison  ~~~  Stratford Digital

     

    Specializing in CadSoft EAGLE

    • Online Sales to North America

    • Electronic Design Services

    • EAGLE Enterprise Toolkit

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 19.06.2012 17:13, James Morrison wrote:

    Tim Gipson wrote on Tue, 19 June 2012 10:50

    >> Hi,

    >> Ran into this strange and potentially dangerous behavior today in EAGLE

    >> 6.0.0 / 6.2.0. If a pin in a library symbol has direction 'Pwr' (possibly

    >> others?), if a net with the same name exists in the schematic, the pin is

    >> being automatically and silently connected in the Board editor (no

    >> visible connection or other indication of this being the case in the

    >> Schematic editor). No questions asked, no warnings, no way to 'undo'

    >> (except by deleting the offending part / rolling back to a point before

    >> the part was introduced, renaming the net, and re-importing the part). If

    >> this has occurred, connecting the actually intended net (if any) to the

    >> pin in the Schematic editor results in shorting the nets together in the

    >> Board editor.

    >>

    >> The fact that only certain pins (notably 'Pwr') are affected suggests

    >> this dangerous behavior may be intentional. Is there any way to a)

    >> disable this behavior, b) generate a loud warning whenever it is

    >> triggered, and/or c) undo the behavior when it is triggered?

    >>

    >> Some specific objections to this being a default behavior:

    >> * Many library part authors (really, many part manufacturers, who

    >> library part authors dutifully copy) use power pin names such as

    >> Vin/Vcc/Vdd/V+ somewhat interchangeably; these names do not uniquely

    >> refer to any voltage standard

    >> * Many schematic authors (including more than one at my day-job)

    >> sometimes use the default names for the 'supply' symbols to designate

    >> different power nets on mixed-voltage boards (e.g. the 'Vcc' symbol for

    >> 5V and 'Vdd' symbol for 3.3V), wreaking havoc with the previous case. You

    >> would never know your part is being overvolted by this behavior (silently

    >> connected to wrong supply), or your supply nets are shorted together,

    >> without careful visual inspection of the ratsnest lines.

    >> * Likewise for ground splitting - I presume (but have not yet tested) a

    >> Pwr pin named 'GND' will exhibit the same behavior, causing a problem

    >> where e.g. a specific part of the circuit requires a split ground (e.g.

    >> AGND), where elsewhere in the design, a library part that does not need,

    >> and should not use the elsewhere AGND offers GND/AGND pins. GND/AGND will

    >> then be shorted together at the 2nd location.

    >> * Nets connected in the Board / design but explicitly shown as

    >> unconnected in the schematic - this should never happen!

    >

    Hello Tim,

     

    This is not a bug, it's a feature!  I know you've heard that before but

    this is actually intended.  Now I agree with you that nothing should ever

    be connected in the PCB that isn't explicitly drawn on the schematic.  But

    this is how EAGLE does it.

     

    From the help for the "PIN" command:

     

    Quote:

    >> If Pwr pins are used on a symbol and a corresponding Sup pin exists on

    >> the schematic, nets are connected automatically.

    >

    My solution is to never, ever, use parts without invoking all gates on all

    parts.  At least then all the pins are visible.

     

    I would like to see a switch to disable this behaviour.  Perhaps an entry

    for the SET command.  CadSoft?

     

    Cheers,

     

    James.

     

     

    Hello Tim, James,

     

    EAGLE connects Pwr pins with same names automatically, that's true.

    Even not invoked Pwr pins will be connected.

    To have this all under control EAGLE runs several checks (ERC).

    For each Pwr signal in the schematic EAGLE wants you to place a

    supply pin on every sheet.

    ERC message: "No supply for power pin xxxxx" helps in identifying

    pwr signals. And there are additional checks on Pwr signals.

    That's the way EAGLE works for about 20 years now......

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    My solution is to never, ever, use parts without invoking all gates on all

    parts.  At least then all the pins are visible.

     

    This is good advice. Unfortunately the "feature" also appears to strike PWR pins which are on the part (don't need to be invoked).

     

    The specific case where I noticed it was adding a battery charger IC which has two PWR pins - "VDD", a generic power source (charge current set by resistor), and "VUSB" for USB port power (charge current 100mA/500mA selectable). One or the other may be left unconnected. Since my application charges from USB port power but the battery requires a custom charge current, I had USB power (appropriately enough named 'VUSB' in the schematic) tied to the VDD pin and the VUSB pin intentionally unconnected. This resulted in the VDD and VUSB pins of the IC being shorted together on the board, with the only indication being the teeny, tiny ratsnest wire between the adjacent pads. It was an extremely lucky catch!

     

    EAGLE connects Pwr pins with same names automatically, that's true.

    Even not invoked Pwr pins will be connected.

     

    I did a quick test today that seems to suggest (n=1 observations) that a PWR pin's auto-connected net will be disconnected again if a different-named net is subsequently wired to the PWR pin. Can you confirm wither the silently auto-connected pins will be (always, sometimes or never) disconnected again if a net with a different name is explicitly connected? Or will the two nets ever both remain connected and become shorted at that pin? (I.e. does the behavior I observed depend on what order the nets/part/connection were created, phase of the moon, etc.?)

     

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    My solution is to never, ever, use parts without invoking all gates on all

    parts.  At least then all the pins are visible.

     

    This is good advice. Unfortunately the "feature" also appears to strike PWR pins which are on the part (don't need to be invoked).

     

    The specific case where I noticed it was adding a battery charger IC which has two PWR pins - "VDD", a generic power source (charge current set by resistor), and "VUSB" for USB port power (charge current 100mA/500mA selectable). One or the other may be left unconnected. Since my application charges from USB port power but the battery requires a custom charge current, I had USB power (appropriately enough named 'VUSB' in the schematic) tied to the VDD pin and the VUSB pin intentionally unconnected. This resulted in the VDD and VUSB pins of the IC being shorted together on the board, with the only indication being the teeny, tiny ratsnest wire between the adjacent pads. It was an extremely lucky catch!

     

    EAGLE connects Pwr pins with same names automatically, that's true.

    Even not invoked Pwr pins will be connected.

     

    I did a quick test today that seems to suggest (n=1 observations) that a PWR pin's auto-connected net will be disconnected again if a different-named net is subsequently wired to the PWR pin. Can you confirm wither the silently auto-connected pins will be (always, sometimes or never) disconnected again if a net with a different name is explicitly connected? Or will the two nets ever both remain connected and become shorted at that pin? (I.e. does the behavior I observed depend on what order the nets/part/connection were created, phase of the moon, etc.?)

     

    Thanks!