Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) 6V Supply
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 642 views
  • Users 0 members are here
Related

6V Supply

e14 Contributor
e14 Contributor over 14 years ago

I couldn't find a +6V supply device to connect to my 7806 voltage regulator

so I thought I'd create my own. I copied the +5V device from the supply2

library to my own library and renamed it as well as the symbol to "6V', but

when I add it to a schematic and try to connect it to a wire the dialog box

which asks me if I want to rename the segment shows "5V"? Where the heck do

I change that?

 

 

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    That was it! It wasn't until I used the Info tool on the pin that I finally

    saw the last "+5V" text - thanks Joern & Tim!

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Am 28.06.2012 03:04, schrieb Ross Waddell:

    I couldn't find a +6V supply device to connect to my 7806 voltage regulator

    so I thought I'd create my own. I copied the +5V device from the supply2

    library to my own library and renamed it as well as the symbol to "6V', but

    when I add it to a schematic and try to connect it to a wire the dialog box

    which asks me if I want to rename the segment shows "5V"? Where the heck do

    I change that?

     

    >

    Your pin NAME simply is still +5V image

    Open you library and in the symbol change the name of the pin.

     

     

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    On Wed, 27 Jun 2012 21:04:02 -0400, Ross Waddell wrote:

     

    I couldn't find a +6V supply device to connect to my 7806 voltage

    regulator so I thought I'd create my own. I copied the +5V device from

    the supply2 library to my own library and renamed it as well as the

    symbol to "6V', but when I add it to a schematic and try to connect it

    to a wire the dialog box which asks me if I want to rename the segment

    shows "5V"? Where the heck do I change that?

     

    Oboy.  I remember having that problem, and solving it, but not the exact

    solution.

     

    If no one coughs up a better answer, go into the library listing for the

    part and go over the pin properties with a fine-toothed comb -- I vaguely

    remember that if you make it a power pin then it wants to force the net

    name to equal the pin name.  Or something like that.

     

    --

    My liberal friends think I'm a conservative kook.

    My conservative friends think I'm a liberal kook.

    Why am I not happy that they have found common ground?

     

    Tim Wescott, Communications, Control, Circuits & Software

    http://www.wescottdesign.com