Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) 4-Layer PCB Stack Up and Internal Planes
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 188 subscribers
  • Views 388 views
  • Users 0 members are here
  • stack
  • drc
  • stackup
  • inner
  • layer
  • polygon
  • 4
Related

4-Layer PCB Stack Up and Internal Planes

e14 Contributor
e14 Contributor over 14 years ago

Hi all,

 

I'm currently working on my first 4-layer design, and I'm having some trouble getting EAGLE to cooperate with me.  First, my layers:

 

1:  TOP

2:  Ground

15:  VDD (+5 VDC)

16:  Bottom

 

I have the stack setup in my DRC as (1+2*15+16) and my layers named Top, GND, VDD, and Bottom.  First, I'm not sure if the stack setup is right for what I want.  I'm going to have components on both sides of the board, so I want to be able to route vias to VDD and GND directly from both the top and bottom layers (is this possible??).  In any case, I still can't even get polygons on the inner layers to fill when I ratsnest.  For example, I create a polygon in the GND layer, and click ratsnest, and nothing happens.  I thought polygons were supposed to behave the same on the inner layers as they do on the outer layers...am I missing something?

 

For reference, I'm using EAGLE 6.2.0 Standard.

 

Thanks in advance.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    On 13.07.2012 17:24, John Wilkins wrote:

    Hi all,

     

    I'm currently working on my first 4-layer design, and I'm having some

    trouble getting EAGLE to cooperate with me.  First, my layers:

     

    1:  TOP 2:  Ground 15:  VDD (+5 VDC) 16:  Bottom

     

    I have the stack setup in my DRC as (12*1516) and my layers named

    Top, GND, VDD, and Bottom.  First, I'm not sure if the stack setup is

    right for what I want.  I'm going to have components on both sides of

    the board, so I want to be able to route vias to VDD and GND directly

    from both the top and bottom layers (is this possible??).  In any

    case, I still can't even get polygons on the inner layers to fill

    when I ratsnest.  For example, I create a polygon in the GND layer,

    and click ratsnest, and nothing happens.  I thought polygons were

    supposed to behave the same on the inner layers as they do on the

    outer layers...am I missing something?

     

    For reference, I'm using EAGLE 6.2.0 Standard.

     

    Thanks in advance.

     

     

     

    Maybe the polygon can't be filled because there are no vias or pads

    belonging to the polygons signal available in the inner layer?

    In this case EAGLE does not know where to connect, and the polygon

    can't be filled.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/