Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Line length change
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 190 subscribers
  • Views 2085 views
  • Users 0 members are here
Related

Line length change

skyflyrr
skyflyrr over 14 years ago

Here is a discussion on the support forum I thought would be good to offer as a suggestion also.

 

The question was:

Is there a way to create a line and specify/change its length once it is on your board layout? I brought up properties on some lines I drew and thought I could specify the length I wanted, but it is not allowed on the properties box? A way to specify after the fact eliminates having to look at coordinates or trying to start at a certain location to determine length. This should be available via a properties menu.

 

 

Answer:

Hi Bob,

 

The length field in the properties box is read-only.  But you can edit the

(x y) coordinate of the start and end of the line so you can effect the

length that way.

 

Or, if you know exactly how much shorter you want it, set the grid to that

exact amount and then move one end of the line by exactly one grid.

 

Cheers,

 

James.

--

James Morrison  ~~~  Stratford Digital

 

Specializing in CadSoft EAGLE

  • Online Sales to North America
  • Electronic Design Services
  • EAGLE Enterprise Toolkit

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

My reply:

James, thank you for the reply. I would like to suggest that in a future version you allow the length to be changed directly on the length box. This is such a useful feature in other cad programs.

 

Thank you,

 

Bob

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to CSWalt

    Walter Spermann <Walter.Spermann@cadsoft.de> wrote:

    Hi James,

     

    On 07/20/12 15:56, Bob Moreno wrote:

    >> Here is a discussion on the support forum I thought would be good to

    >> offer as a suggestion also.

    >>

    >> The question was:

    >> Is there a way to create a line and specify/change its length once it is

    >> on your board layout? I brought up properties on some lines I drew and

    >> thought I could specify the length I wanted, but it is not allowed on

    >> the properties box? A way to specify after the fact eliminates having to

    >> look at coordinates or trying to start at a certain location to

    >> determine length. This should be available via a properties menu.

    >>

    >>

    >> Answer:

    >> Hi Bob,

    >>

    >> The length field in the properties box is read-only.  But you can edit the

    >> (x y) coordinate of the start and end of the line so you can effect the

    >> length that way.

    >>

    >> Or, if you know exactly how much shorter you want it, set the grid to that

    >> exact amount and then move one end of the line by exactly one grid.

    >>

    >> Cheers,

    >>

    >> James.

    In EAGLE's property dialogs generally all properties are just changeable in one way

    and only get effective after apply or ok pressed.

    This makes the behaviour very clear.

     

    Your suggestion basically makes sense of course. But with this you'd be

    able to change cordinates

    in 2 ways (by changing coordinates directly and/or changing length).

    If both is changed, who wins ? What if additionally the curve value is changed ?

     

    If only length is changed, we could keep the wire's first point and change the 2nd point

    or the other way. That's not clear either. There needs to be something

    like a swap option, too.

    The dialog will no more be so easy to understand, so I'm not sure

    if that's such a good idea.

     

    Regards,

    Walter Spermann

     

     

    Now that was a lazy answer image

    How about a calculate button on each point inside the properties? Put angle

    and length (load it with current) in a requester and it calculates the new

    point for you. There is no need to support command line, but I guess it

    would be nice there too.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • skyflyrr
    skyflyrr over 14 years ago in reply to CSWalt

    I constantly need to draw lines on the tplace layer and I have no way to be sure lines that are not near each other are the same length.I currently have to draw a line from location 0,0,0, or calculate coordinates, add/subtract etc, (for length measurements) and then move it to where I need it. This however creates the problem of needing to work at inserting the lines at the precise location I need them, rather than just create a line from where I need and simply specify the length. I realize I can start a line anywhere, but to be precise as to length and match other lines I need is very time consuming. This line drawing with a length measurement would also go a long way in helping to create outlines in the library package edit area by allowing an outline to be done simply by drawing lines to length needed no matter where they start. And yes I mean leave the  first point and only change the second point as it relates to what length you specify. Of course allowing normal right mouse click rotation on the line also. I know I mention WinQcad (no longer supported) a lot here but if you look at the way lines and packages are made in that program you get a good idea how easy it is to draw lines, make packages etc. of course Eagle exceeds that program in so many ways, but in some WinQcad is easier to use. The package edit in WinQcad is using this line draw concept I mention here by just needing to specify X and Y length along with pitch and row or colunm count to create pads of any shape and count in seconds.

     

    Regards,

     

    Bob Moreno

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • CSWalt
    CSWalt over 14 years ago

    Hi James,

     

    On 07/20/12 15:56, Bob Moreno wrote:

    Here is a discussion on the support forum I thought would be good to offer as a suggestion also.

     

    The question was:

    Is there a way to create a line and specify/change its length once it is on your board layout? I brought up properties on some lines I drew and thought I could specify the length I wanted, but it is not allowed on the properties box? A way to specify after the fact eliminates having to look at coordinates or trying to start at a certain location to determine length. This should be available via a properties menu.

     

     

    Answer:

    Hi Bob,

     

    The length field in the properties box is read-only.  But you can edit the

    (x y) coordinate of the start and end of the line so you can effect the

    length that way.

     

    Or, if you know exactly how much shorter you want it, set the grid to that

    exact amount and then move one end of the line by exactly one grid.

     

    Cheers,

     

    James.

    In EAGLE's property dialogs generally all properties are just changeable in one way

    and only get effective after apply or ok pressed.

    This makes the behaviour very clear.

     

    Your suggestion basically makes sense of course. But with this you'd be able to change cordinates

    in 2 ways (by changing coordinates directly and/or changing length).

    If both is changed, who wins ? What if additionally the curve value is changed ?

     

    If only length is changed, we could keep the wire's first point and change the 2nd point

    or the other way. That's not clear either. There needs to be something like a swap option, too.

    The dialog will no more be so easy to understand, so I'm not sure

    if that's such a good idea.

     

    Regards,

    Walter Spermann

     

    --

    -


    Walter Spermann

    Softwareentwicklung

    CadSoft Computer GmbH

    Pleidolfweg 15

    84568 Pleiskirchen

    Tel.: 08635/6989-10

    www.cadsoft.de

    -


    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschäftsführer: Thomas Liratsch

    -