Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Determining pin pitch for existing library parts
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 190 subscribers
  • Views 1909 views
  • Users 0 members are here
Related

Determining pin pitch for existing library parts

Krycek
Krycek over 14 years ago

I am very new to Eagle so still finding my way around it. One thing that currently has me confused is how to determine the pin pitch for a footprint thats in the library.

 

In this case I am using an F25HP package from the con-subd.lbr on a simple parallel breakout PCB im laying out but for the life of me I can't see a way either in the PCB layout or the library editor itself to determine the pin pitch that has been used for this package.

 

Any help would be appreciated as I can see me running into similar problems with other library packages that aren't on a standard 0.1" pitch.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    On 7/31/2012 5:54 AM, Krycek wrote:

    I am very new to Eagle so still finding my way around it. One thing that currently has me confused is how to determine the pin pitch for a footprint thats in the library.

     

    In this case I am using an F25HP package from the con-subd.lbr on a simple parallel breakout PCB im laying out but for the life of me I can't see a way either in the PCB layout or the library editor itself to determine the pin pitch that has been used for this package.

     

    Any help would be appreciated as I can see me running into similar problems with other library packages that aren't on a standard 0.1" pitch.

     

     

    You could...

     

    1.  Adjust the grid settings (Turn it on if its not visible) to

    something on the order of what you expect for the pin pitch then eyeball

    it to get a rough idea.

     

    2.  Open the library with the library editor,  pick the info command

    tool, and select one of the holes/pads.   The info dialog will show you

    the exact position of the hole/pad.    Note the coordinates and then

    select an adjacent hole/pad.   Subtract the coordinates to get the pitch.

     

    3.  Use the Mark tool to set a marker at one pin/pad.   After you set

    the marker there should be a relative coordinate readout in the upper

    left part of the window frame/tool bars.   The Relative coordinate will

    be in the units of the current grid and will show you how far the mouse

    pointer/cursor is from the marker.    You way want to hold down the Alt

    key to use the alt grid for fine positioning.

     

    Regards,

    Jim

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • skyflyrr
    skyflyrr over 14 years ago in reply to e14 Contributor

    Seems like a lot of trouble to know the pitch of a component? Why not have this information available in a description of the part. Any part should have pad size, pitch and all other relevent information in a pop-up on request. After all if the part exists, the info exists.

     

    One other thing, even if the part description mentions the pitch and other package information, there could be a mistake. I always measure pitch and pad sizes just to be sure. Most times the only way to be sure you get what you need is to make the part layout yourself.

     

     

    Regards,

     

    Bob Moreno

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to skyflyrr

    On 7/31/2012 9:33 AM, Bob Moreno wrote:

    Seems like a lot of trouble to know the pitch of a component? Why not have this information available in a description of the part. Any part should have pad size, pitch and all other relevent information in a pop-up on request. After all if the part exists, the info exists.

     

     

    Hi Bob,

     

    The truth is that not everyone who makes libraries has the presence of

    mind to include such information. I wrote a small standard for library

    creation to try to elevate the overall quality of user submitted libraries.

     

    One of the recommendations is to include a link to the datasheet or some

    other documentation which can provide the finer details of a part.

     

    You can find it under the Documentation section of:

     

    www.cadsoftusa.com/downloads

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to skyflyrr

    On 7/31/2012 9:33 AM, Bob Moreno wrote:

    Seems like a lot of trouble to know the pitch of a component? Why not have this information available in a description of the part. Any part should have pad size, pitch and all other relevent information in a pop-up on request. After all if the part exists, the info exists.

     

     

    Hi Bob,

     

    The truth is that not everyone who makes libraries has the presence of

    mind to include such information. I wrote a small standard for library

    creation to try to elevate the overall quality of user submitted libraries.

     

    One of the recommendations is to include a link to the datasheet or some

    other documentation which can provide the finer details of a part.

     

    You can find it under the Documentation section of:

     

    www.cadsoftusa.com/downloads

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • skyflyrr
    skyflyrr over 14 years ago in reply to e14 Contributor

    Hi Jorge, I saw and read your write-up, very helpful, thanks.

     

    Regards,

     

    Bob Moreno