Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Use the .com extension for the command line executable on Windows
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 190 subscribers
  • Views 1584 views
  • Users 0 members are here
Related

Use the .com extension for the command line executable on Windows

e14 Contributor
e14 Contributor over 14 years ago

A usual problem when compiling programs on Windows is that GUI executables cannot write to the command line from which they are started. To do that you have to compile them as Console executables, but then there is always an annoying command line window poping up when running it from a shortcut.

 

The solution is to ship two executables, one compiled as GUI, one as Console, and that is what Eagle is doing. The GUI executable is eagle.exe, and the Console executable is eaglecon.exe.

 

An informal convention when using that dual executable solution is to use the same base name for the two files, but using the .com extension for the Console executable. This has the advantage that you only have a single name to document and remember ("eagle"), but thanks to the default order of extensions in the Pathext environment variables, eagle.com has priority over eagle.exe when run from a command line (and one can still explicitly run the GUI version by typing "eagle.exe"). In shortcuts the full path to the .exe is necessary anyway, so it's not a problem to have a "conflicting" .com file. This convention is used for example by the Microsoft Visual Studio IDE (devenv.exe for shortcuts, devenv.com for command line use and scripting), or the Inkscape open source vector graphics editor (inkscape.exe for shortcuts, inkscape.com for command line use and scripting).

 

My suggestion is then to simply rename the file "eaglecon.exe" to "eagle.com".

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Jérôme Vuarand wrote on Wed, 01 August 2012 12:50

    An informal convention when using that dual executable solution is to

    use the same base name for the two files, but using the .com extension

    for the Console executable.

     

    There is no such convention.  Furthermore, the file name suffix ".com"

    already has a specific meaning.

     

    Quote:

    My suggestion is then to simply rename the file "eaglecon.exe" to

    "eagle.com".

     

    Really bad idea.

     

    Some other convention could be used though.  For example, I add "_w" to GUI

    executables, like myprog.exe for the command line and myprog_w.exe for the

    window version.  You want the command line version to be the simple name

    since you have to type it.  The GUI version can be more convoluted since it

    is generally run from a menu item with the actual executable name hidden

    from the user.

     

    The Eagle convention is fine too.  The point is there is no standard, just

    various things people have done.  There is also little need for one.  There

    is no problem to solve here.  Let's move along and stop diverting the

    developer's attention on frivolous issues like this.

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Olin Lathrop wrote:

    Really bad idea.

    Telling something is a bad idea mandates some explanation. Otherwise it's just an opinion, and I don't think your opinion matters nearly as much as the one from the Microsoft Visual Studio team.

    Olin Lathrop wrote:

    There is no problem to solve here.  Let's move along and stop diverting the developer's attention on frivolous issues like this.

    There may be no problem for you, that's a problem for me. Anyways the forum is named "suggestions", not "bug reports", and even if there is no problem that's a place to propose improvements. So I will kindly ignore your message and continue "diverting the developer's attention" on issues like this.

     

    Walter Spermann wrote:

    I agree. It's difficult to make everybody happy on questions like this. As long there is no real need to change that we keep it.

    Fair enough. My goal was just to improve consistency with other platforms where I assume a single "eagle" binary name is used, and with other applications that use a different naming convention on Windows to solve the same problem. Of course that was never meant as a high priority request, just a personal opinion.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Olin Lathrop wrote:

    Really bad idea.

    Telling something is a bad idea mandates some explanation. Otherwise it's just an opinion, and I don't think your opinion matters nearly as much as the one from the Microsoft Visual Studio team.

    Olin Lathrop wrote:

    There is no problem to solve here.  Let's move along and stop diverting the developer's attention on frivolous issues like this.

    There may be no problem for you, that's a problem for me. Anyways the forum is named "suggestions", not "bug reports", and even if there is no problem that's a place to propose improvements. So I will kindly ignore your message and continue "diverting the developer's attention" on issues like this.

     

    Walter Spermann wrote:

    I agree. It's difficult to make everybody happy on questions like this. As long there is no real need to change that we keep it.

    Fair enough. My goal was just to improve consistency with other platforms where I assume a single "eagle" binary name is used, and with other applications that use a different naming convention on Windows to solve the same problem. Of course that was never meant as a high priority request, just a personal opinion.