Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Revise the pricing policy
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 189 subscribers
  • Views 445 views
  • Users 0 members are here
Related

Revise the pricing policy

e14 Contributor
e14 Contributor over 14 years ago

Hello,

 

To make a long story short, my company will disapear in two or three years. I've been designing all sort of electronic devices for about 30 years, using OrCAD, Protel, and Altium (the later for almost 10 years).

Of course I will continue to practice my job, probably as self employed, in the field of high-end audio amplifiers and such, a field that has been a hobby since school.

 

My problem is that I like tubes (or valves if you prefer). When it comes to size this technology is exactly the contrary of the nowadays trends. No valves in SMD, no Sir !

 

Of course I could continue to use my Altium license, but to keep it up to date costs a lot of money, and if it's acceptable for a company making profit from it, it will be unacceptable for a very small one like my future one.

 

I feel that there should be something between the small van (standard Eagle - 100x160 mm) and the 200 Tons Mine Hauler (pro - 4000x4000 mm - Christ! who makes such huge boards ?).

Maybe a simple sturdy pick-up, allowing 6 layers and something like 200x200 mm routing area ? Or even better: turn the simple van into a great pick-up and allow the standard version to work on a 200x200mm area.

 

I'd rather work with Eagle, but other packages are on the market, lower priced (or even free) allowing 1000x1000 or even more.

 

Best regards,

 

Jacques

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Op Thu, 09 Aug 2012 12:01:10 +0200 schreef Jacques Casier 

    <noreply-121859@element14.com>:

     

    Hello,

     

    To make a long story short, my company will disapear in two or three 

    years. I've been designing all sort of electronic devices for about 30 

    years, using OrCAD, Protel, and Altium (the later for almost 10 years).

    Of course I will continue to practice my job, probably as self employed, 

    in the field of high-end audio amplifiers and such, a field that has 

    been a hobby since school.

     

    My problem is that I like tubes (or valves if you prefer). When it comes 

    to size this technology is exactly the contrary of the nowadays trends. 

    No valves in SMD, no Sir !

     

    Of course I could continue to use my Altium license, but to keep it up 

    to date costs a lot of money, and if it's acceptable for a company 

    making profit from it, it will be unacceptable for a very small one like 

    my future one.

     

    I feel that there should be something between the small van (standard 

    Eagle - 100x160 mm) and the 200 Tons Mine Hauler (pro - 4000x4000 mm - 

    Christ! who makes such huge boards ?).

    Maybe a simple sturdy pick-up, allowing 6 layers and something like 

    200x200 mm routing area ? Or even better: turn the simple van into a 

    great pick-up and allow the standard version to work on a 200x200mm area.

     

    I'd rather work with Eagle, but other packages are on the market, lower 

    priced (or even free) allowing 1000x1000 or even more.

     

    Best regards,

     

    Jacques

     

     

     

    Hi,

     

    I don't think a change in licensing choices will be very likely, but just 

    in case, I'd like to support your request.

     

    I also design (HiFi / High end) audio gear, mainly based on tubes. And 

    yes, that means I need size and only use moderate complexity. I did this 

    when I bought Eagle pro (> 10 years ago) and still like the way it works. 

    I don't use or have a license for the autorouter.

    Understandably, Eagle development concentrates on modern technology, and 

    that's fine. I don't want the product to change, like it fine as it is, 

    but like you, would welcome a more flexible pricing scheme. Because most 

    of the added features aren't really neccesary for me, a flexible pricing 

    scheme would allow me to convince myself to keep using and updating Eagle, 

    instead of looking for something else.

     

    I don't even need 6 layers, 4 would be enough, and if the price is right I 

    could even accept 2 layer and change some design decisions. But a larger 

    board area would be very welcome. Something like 4 Eurocards (200mm x 

    320mm) sounds about right.

     

    /DREAM_MODE_OFF

     

     

    Richard

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Here's a suggestion inspired by Adobe! Rental licenses.... meaning when you need to make a 300mm x 300mm board, you can rent this upgrade for a month at a time! Then you get the best of both worlds. Adobe now does this with their entire Creative Suite CS6 (which is very expensive to purchase otherwise).

     

    Also, the great thing is no commitment.

     

    Anyway, just my thoughts...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 13 years ago in reply to e14 Contributor

    You could look at EasyPC which has low cost versions based on pin count rather than board size so the 1000 pin limited version is only £247. I've used EasyPC for years and while of course it's not perfect I've found it good enough for some quite complex designs. The good news is that I've found it to have far fewer bugs than more exotic packages - and it is easy to use.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 13 years ago in reply to e14 Contributor

    You could look at EasyPC which has low cost versions based on pin count rather than board size so the 1000 pin limited version is only £247. I've used EasyPC for years and while of course it's not perfect I've found it good enough for some quite complex designs. The good news is that I've found it to have far fewer bugs than more exotic packages - and it is easy to use.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to michaelkellett

    Op Tue, 28 Aug 2012 09:42:02 +0200 schreef Michael Kellett 

    <noreply-5400@element14.com>:

     

    You could look at EasyPC which has low cost versions based on pin count 

    rather than board size so the 1000 pin limited version is only £247. 

    I've used EasyPC for years and while of course it's not perfect I've 

    found it good enough for some quite complex designs. The good news is 

    that I've found it to have far fewer bugs than more exotic packages - 

    and it is easy to use.

     

    MK

     

     

    Thanks, I know there's other pcb software with licensing schemes that are 

    probably better suited for my needs. In fact, I tried EasyPC, among 

    others, last time I was looking for new pcb layout software. Can't really 

    remember why it didn't work for me (was 10 years ago....).

     

    The problem is, with cad software, there is almost no compatability 

    between different manufacturers, or only very basic. I've used Eagle for 

    more than 10 years (and used other software before that). I've made 

    hundreds of pcb's with it and with audio / tube stuff, I regularly 

    rework/expand pcb's made 10 years ago. The technology doesn't age that 

    much.

     

    One very important reason why I choose Eagle over others is, that even 10 

    years ago, it already existed for a long time and looked very stable with 

    a promising future. The price (for the pro version), although a bit steep 

    for a 'pro-hobbyist', does allow Cadsoft to continue development better 

    than some of the cheap packages, which feature-wise could be good enough 

    for me.

     

    So, I would like to work with Eagle as long as possible. But lot's of the 

    added features are not very useful for me and adding some form of 

    licensing for "less features - more pcb size" would help a lot with that 

    decision!

     

     

    Richard