EAGLE User Support (English) How to change power pin connection on logic chip library
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
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 518 views
  • Users 0 members are here
Related

How to change power pin connection on logic chip library

Former Member
Former Member over 13 years ago

I have a circuit that can run from 18V to 32v but has a digital switching system with a decoder and other arrangements of logic gates.  I have a power suply setup that will always derive a +5v terminal to all the digital serctions of the circuit.  The problem is eagle's default library automaticlly defaults the power and ground pins to the main power and ground and has no option to wire those pins in the schematic.  I went to the library and changed the pins from pwr to passive hopping that it will allow for the power and ground connections to show in the schematic but to no avail.  With the complexity of the circuit I do not want to manually route the digital VCC from the other 2 power supplies in the circuit in fear that I will make a small error in the board which will indeed be costly.  Is there anyway I can change the subnet of the power pins on the logic family chips to that which I desire?  When I go into properties and change the subnet of a logic power pin to the same subnet of the +5v DC power supply out, it also changes the subnet of the main power supply to +5V and still does not connect that line to the digital supply.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 13 years ago

    Justin Moss wrote:

    >I have a circuit that can run from 18V to 32v but has a digital

    >switching system with a decoder and other arrangements of logic

    >gates.  I have a power suply setup that will always derive a +5v

    >terminal to all the digital serctions of the circuit.  The problem is

    >eagle's default library automaticlly defaults the power and ground

    >pins to the main power and ground and has no option to wire those pins

    >in the schematic. [...]

     

    help invoke

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 13 years ago

    Justin Moss wrote:

    >I have a circuit that can run from 18V to 32v but has a digital

    >switching system with a decoder and other arrangements of logic

    >gates.  I have a power suply setup that will always derive a +5v

    >terminal to all the digital serctions of the circuit.  The problem is

    >eagle's default library automaticlly defaults the power and ground

    >pins to the main power and ground and has no option to wire those pins

    >in the schematic. [...]

     

    help invoke

    --

     

    Lorenz