Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) drillegend troubles
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 189 subscribers
  • Views 372 views
  • Users 0 members are here
Related

drillegend troubles

fritzz
fritzz over 13 years ago

I am tryng to use the drillegend-2.ulp and am getting a weird result.

 

It looks like when I look at layer 144 that the drills are in the right place, but the table below shows them MUCH too large.

It shows drills are 26mm, 32mm, 33mm, and 126mm. I don't think my drills are that big.

 

Help! Do I need to do something before running this?

 

Is there a betetr way to check my drills locations/sizes?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to fritzz

    d r wrote:

    So drill legend2 is old, and drilllegend stack is the the only one to

    use these days??

     

    Each and every ULP is coded with a version of Eagle in mind. Many are not

    backwards compatible and many inform you about this when you attempt to run

    them in an older version. Not all do.

     

    The assumption to date was that they would all be forwards compatible. With

    the arrival of v6 that all went out the window due to the use of different

    internal units used by v6. This trips up some of the older ULPs as they

    perform calculations based on the internal unit size of the earlier

    versions. So now we need to accept that there are v5 ULPs that will work in

    v6 but there are also v5 ULPs that won't.

     

    If you are using ULPs  other than those included with your version of Eagle

    you should be wary of them giving incorrect results.

     

     

    HTH

    Warren.

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fritzz
    fritzz over 13 years ago in reply to e14 Contributor

    So drill legend2 is old, and drilllegend stack is the the only one to use these days??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to fritzz

    d r wrote:

    I saw a message now from a year ago implying that maybe this is bug

    and that 6.2 does not work with this ULP.

     

    From the ULPs that are included with 6.2.2 try drillegend-stack.ulp

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fritzz
    fritzz over 13 years ago

    I saw a message now from a year ago implying that maybe this is bug and that 6.2 does not work with this ULP.