Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) custom line width?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 189 subscribers
  • Views 455 views
  • Users 0 members are here
Related

custom line width?

fritzz
fritzz over 13 years ago

When I'm making a symbol, each time I like to have a line that's .005 wide. but the menu doesn't have that number

Yes I can add it, but them when I restart it's gone,

 

How do I add a custom number to that series of widths? Something in  eagle.scr?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Am 18.09.2012 05:26, schrieb d r:

    When I'm making a symbol, each time I like to have a line that's .005 wide. but the menu doesn't have that number

    Yes I can add it, but them when I restart it's gone,

     

    How do I add a custom number to that series of widths? Something in  eagle.scr?

     

    Yes. Put a line like

       SET Width_Menu 0 0.006 0.01 0.016 0.025 0.03 0.04 0.05 0.1 0.2;

    in your eagle.scr file, then the menu will show ONLY the above entries.

     

    Andreas Weidner

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fritzz
    fritzz over 13 years ago in reply to e14 Contributor

    very good, thanks.

     

    I notice that some widths can't be defined, for example

     

    BRD:

    SET WIDTH_MENU 0 .005 0.01 0.012 .016 .024 0.032 0.04 0.05 .056 .066 .07 .086 .1 .15 .252;

     

    will not add a .005 to the board editor menu.

     

    If you pasted that same text straight into the command line in the board editor, then it woudl add .005

     

    Bug?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fritzz
    fritzz over 13 years ago in reply to e14 Contributor

    very good, thanks.

     

    I notice that some widths can't be defined, for example

     

    BRD:

    SET WIDTH_MENU 0 .005 0.01 0.012 .016 .024 0.032 0.04 0.05 .056 .066 .07 .086 .1 .15 .252;

     

    will not add a .005 to the board editor menu.

     

    If you pasted that same text straight into the command line in the board editor, then it woudl add .005

     

    Bug?