EAGLE User Support (English) Through hole parts connected to the top layer
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
  • Replies 7 replies
  • Subscribers 182 subscribers
  • Views 2368 views
  • Users 0 members are here
Related

Through hole parts connected to the top layer

Plecto
Plecto over 13 years ago

Hi. I'm trying to make a board and then send it off to a board house for etching. I made the autorouter make the traces for me, both top and bottom traces with vias and all. The thing is that I have both SMT parts and through-hole parts on my board, but the autorouter doesn't seem to care. It sends top layer traces to my through-hole parts, how do I fix this?

  • Sign in to reply
  • Cancel
Parents
  • jvdberg@ieee.org
    jvdberg@ieee.org over 12 years ago

    Through-hole parts can be connected to traces on the component layer if plated through holes are used. However if this is done, some parts are difficult to remove without damaging the board. Heavy components like transformers might break from the board if only connected to traces on the component side. Components that need a lot of heat during the soldering process might not properly soldered if  traces at the component side remove part of the heat and only a small surface is available to apply the heat. Connectors, switches and  potmeters might damage the board as a result of mechanical forces applied to that component. It would be nice if the auto router had the possibility to connect selected parts only at the solder side. It would also be nice if connectors, switches and  potmeters could be connected to wider traces. Very often the traces to these components break as a result of mechanical forces. For instance the earphone connector of a portable MP3 player. A wide trace can easily be repaired by soldering a piece of wire over the crack. This cannot be done by selecting the board rules to use wider traces. The auto router should use wide traces  only close to those components and only where board space is available. This way the boards are more reliable and easier to repair.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jvdberg@ieee.org
    jvdberg@ieee.org over 12 years ago

    Through-hole parts can be connected to traces on the component layer if plated through holes are used. However if this is done, some parts are difficult to remove without damaging the board. Heavy components like transformers might break from the board if only connected to traces on the component side. Components that need a lot of heat during the soldering process might not properly soldered if  traces at the component side remove part of the heat and only a small surface is available to apply the heat. Connectors, switches and  potmeters might damage the board as a result of mechanical forces applied to that component. It would be nice if the auto router had the possibility to connect selected parts only at the solder side. It would also be nice if connectors, switches and  potmeters could be connected to wider traces. Very often the traces to these components break as a result of mechanical forces. For instance the earphone connector of a portable MP3 player. A wide trace can easily be repaired by soldering a piece of wire over the crack. This cannot be done by selecting the board rules to use wider traces. The auto router should use wide traces  only close to those components and only where board space is available. This way the boards are more reliable and easier to repair.