EAGLE User Support (English) support for microstrip RF design
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
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 518 views
  • Users 0 members are here
  • eagle
  • qucs
  • layout
  • support
  • microstrip
  • Design
  • rf
Related

support for microstrip RF design

Former Member
Former Member over 13 years ago

For the wishlist...

 

It would be really cool to have eagle support for high-frequency RF design and if possible, the ability to read directly from qucs file formats.  Qucs is open-source, has a text-based file format, and supports simulation of several types of microstrip.  The current types of supported microstrip distributed components and associated equations are described in this link.

http://qucs.sourceforge.net/tech/node74.html

 

Would also be nice to also be able to click on a 2-port node in the eagle pcb layout, associate a touchstone s-parameter file for each end of the node, and be able to do a frequency / s-parameter plot in dB.  If the associations remained persistent for a design,  then maybe you could even analyze a complete set of nodes  (the entire tx path or rx path for example).

 

Maybe some tools to synthesize optimal matches in microstrip?

 

Just some thoughts..

  • Sign in to reply
  • Cancel
Parents
  • Joop14
    Joop14 over 10 years ago

    I would like to put this again under the attention of the Cadsoft team.

     

    I too believe that a (two-way) connection between Eagle and Qucs would be a big win for Eagle users.

     

    https://en.wikipedia.org/wiki/Quite_Universal_Circuit_Simulator

     

    Kind Regards,

     

    Joop

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to Joop14

    Hi Joop,

     

    I've played with Qucs before and it's a very interesting simulator. As

    you know we have an interface for LTSpice which is Free (as in beer not

    as in speech), which covers that need very well.

     

    Qucs is a bit niche, and I don't know how many users would benefit from

    such an interface but I'll post it to the Devs anyway and they'll make a

    determination.

     

    Thanks for the suggestion.

     

    Best Regards,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 10 years ago in reply to Joop14

    Hi Joop,

     

    I've played with Qucs before and it's a very interesting simulator. As

    you know we have an interface for LTSpice which is Free (as in beer not

    as in speech), which covers that need very well.

     

    Qucs is a bit niche, and I don't know how many users would benefit from

    such an interface but I'll post it to the Devs anyway and they'll make a

    determination.

     

    Thanks for the suggestion.

     

    Best Regards,

    Jorge Garcia