Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Utility for package creation
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 190 subscribers
  • Views 926 views
  • Users 0 members are here
Related

Utility for package creation

cosborne2000
cosborne2000 over 13 years ago

Does Eagle have a utility for the creation of typical packages?

 

I'm looking for something that you input pin pitch, row spacing, total pin count, and other standard dimensions and have the program generate a good starting point.

I tried the createsymsmdpackage_rel2 ULP but it aborts with a syntax error (Eagle version 6.2).

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    I recently bought the new & improved PCB Footprint Expert (FPX) from PCB

    Libraries. For $200 you get an excellent script generator that is

    IPC-7351C-compliant in pads/lands/silkscreen/nomenclature, and other stuff.

    It produces a .scr file you can then run in Eagle to synthesize the part in

    your open Eagle library.

     

    I don't work for PCB Libraries, but have provided debug feedback for the

    helpful and courteous developers. I expect them to issue a patch or update

    soon for the current 2012.23 release, so be sure to check with them to

    ensure you get the latest. Make you sure you spec the EAGLE-output version,

    and pay by Paypal/Credit Card if you don't want to wait a week for the

    e-check to clear.

     

    /AT

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • skyflyrr
    skyflyrr over 13 years ago in reply to e14 Contributor

    I can see that buying another program to create packages is one answer, other programs of half the cost include great package creation as standard. Again I state that Eagle should include within the package editor a menu item to create pads by X and Y size entry, pad count in either rows or colums, and pitch of pads. I use a much less expensive program just for the reason of it's package creation abilities whenever possible. I know Eagle is much more capable in most other areas, but package creation is not one of them, but should be.Why should we have to call up a scrip, buy another program, constantly need to change grid sizes or any number of other items just to build a package?

     

    I understand this post is better in the suggestion area, but when I see people having such problems with package creation, I can't help but throw in my two cents worth.

     

    Thanks,

     

    Bob Moreno

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to skyflyrr

    I was a PADS user for a number of years, and almost nothing could be clunkier in the building of schematic and PCB entities. Despite this PADS remains a great favorite in the OrCAD-PADS mixed environment.

     

    With the worst of the EAGLE script-generation bugs worked out of the FPX 2012.24 release, it's a time-saver now to generate best-practice PCB lands, and good and consistent silk and assembly art.

     

    NB the requirements of the IPC-7351C standard are actually pretty useful, one of them being that silk screened under the placed package is useless, so why draw it in the first place? Also pin 1 ID is needed for engineers and techs to get oriented for instrumentation, and for inspectors to quickly verify correct placement rotation. I might point out that the C-generated script SMD footprint images posted earlier fail on both these counts.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to skyflyrr

    I was a PADS user for a number of years, and almost nothing could be clunkier in the building of schematic and PCB entities. Despite this PADS remains a great favorite in the OrCAD-PADS mixed environment.

     

    With the worst of the EAGLE script-generation bugs worked out of the FPX 2012.24 release, it's a time-saver now to generate best-practice PCB lands, and good and consistent silk and assembly art.

     

    NB the requirements of the IPC-7351C standard are actually pretty useful, one of them being that silk screened under the placed package is useless, so why draw it in the first place? Also pin 1 ID is needed for engineers and techs to get oriented for instrumentation, and for inspectors to quickly verify correct placement rotation. I might point out that the C-generated script SMD footprint images posted earlier fail on both these counts.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 13 years ago in reply to e14 Contributor

    Hi Alex,

     

    For those that are hand-soldering, a footprint that draws the outline of the package (call it "under the package" if you will) is actually quite important for the simple reason that it acts as an aid to be able to visually center the package to the footprint. The C program asks for the width of the package to achieve this.

    I understand that pick-and place machines do not require an outline.

     

    If one desires the outline around the package, I don't think it takes a genius to modify the C code, since I provided the source. In fact you may not need to do anything for the quad style packages, because you could type a width greater than the package size.

     

    You've missed the main point of the code, which is to generate all the pads in the correct position. Moving the round spot which marks pin 1 is

    a trivial affair that I can achieve with my mouse and a single click-and-drag operation. Or modify the source code. It is code written in an

    afternoon; hardly difficult, but they save a lot of time.

     

    And getting practice with the EAGLE scripts is no bad thing, because you can generate complex shapes if needed - I like my toroids to exactly fit PCBs.

    Maybe third party products do that, but I don't know.

     

    Or one could spend $200 on a package, but for now, I'm very happy with the time I'm saving (and I've created hundreds of boards).

     

    But yes, I totally agree with the poster earlier that we should not need ancillary software to achieve this purpose. It is functionality that should

    be in EAGLE. I posted such a recommendation here.