Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Problem with "Restring"
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 188 subscribers
  • Views 1330 views
  • Users 0 members are here
Related

Problem with "Restring"

e14 Contributor
e14 Contributor over 13 years ago

I am using Eagle 6.2.0 Professional, on Windows 7

 

 

I need to change the size of the annular ring (restring)

around two specific pads in a component.  The library for the

part lets me turn off "auto" and choose the size of the

restring for the two pads.  So, I can make the library

footprint for the part look like the part as I want it

on the board.

 

Then Eagle, when placing the part, ignores the library

as built and uses the "global" (or default) percentage restring

in the Design Rules over-riding the desired restring sizes

in the library.

 

I want to use the global settings for the other several thousand pads

and vias in the board. (It is a big board)  I don't want to change

them all to the smaller restring I need in this one place.

 

Searching the email history, I find a long discussion by Richard Hammerl

from November 25, 2008 saying this is not possible in Eagle 4 and 5.

 

Is this possible in Eagle 6.2?

 

--- Graham

 

==

 

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    On 11.10.2012 18:53, Graham wrote:

    I am using Eagle 6.2.0 Professional, on Windows 7

     

    >

    I need to change the size of the annular ring (restring)

    around two specific pads in a component.  The library for the

    part lets me turn off "auto" and choose the size of the

    restring for the two pads.  So, I can make the library

    footprint for the part look like the part as I want it

    on the board.

     

    Then Eagle, when placing the part, ignores the library

    as built and uses the "global" (or default) percentage restring

    in the Design Rules over-riding the desired restring sizes

    in the library.

     

    I want to use the global settings for the other several thousand pads

    and vias in the board. (It is a big board)  I don't want to change

    them all to the smaller restring I need in this one place.

     

    Searching the email history, I find a long discussion by Richard Hammerl

    from November 25, 2008 saying this is not possible in Eagle 4 and 5.

     

    Is this possible in Eagle 6.2?

     

    --- Graham

     

    ==

     

    >

     

    Graham,

     

    the situation in EAGLE 6 is the same as it was in version 4 or 5.

    The pad diameter always obeys at least the minimum value that is

    given for the width of the copper ring around the drilling in the

    Design Rule's restring settings.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    On 11.10.2012 18:53, Graham wrote:

    I am using Eagle 6.2.0 Professional, on Windows 7

     

    >

    I need to change the size of the annular ring (restring)

    around two specific pads in a component.  The library for the

    part lets me turn off "auto" and choose the size of the

    restring for the two pads.  So, I can make the library

    footprint for the part look like the part as I want it

    on the board.

     

    Then Eagle, when placing the part, ignores the library

    as built and uses the "global" (or default) percentage restring

    in the Design Rules over-riding the desired restring sizes

    in the library.

     

    I want to use the global settings for the other several thousand pads

    and vias in the board. (It is a big board)  I don't want to change

    them all to the smaller restring I need in this one place.

     

    Searching the email history, I find a long discussion by Richard Hammerl

    from November 25, 2008 saying this is not possible in Eagle 4 and 5.

     

    Is this possible in Eagle 6.2?

     

    --- Graham

     

    ==

     

    >

     

    Graham,

     

    the situation in EAGLE 6 is the same as it was in version 4 or 5.

    The pad diameter always obeys at least the minimum value that is

    given for the width of the copper ring around the drilling in the

    Design Rule's restring settings.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    CadSoft Support wrote on Tue, 16 October 2012 06:40

    On 11.10.2012 18:53, Graham wrote:

    I am using Eagle 6.2.0 Professional, on Windows 7

     

     

    I need to change the size of the annular ring (restring)

    around two specific pads in a component.  The library for the

    part lets me turn off "auto" and choose the size of the

    restring for the two pads.  So, I can make the library

    footprint for the part look like the part as I want it

    on the board.

     

    Then Eagle, when placing the part, ignores the library

    as built and uses the "global" (or default) percentage restring

    in the Design Rules over-riding the desired restring sizes

    in the library.

     

    I want to use the global settings for the other several thousand

    pads

    and vias in the board. (It is a big board)  I don't want to change

    them all to the smaller restring I need in this one place.

     

    Searching the email history, I find a long discussion by Richard

    Hammerl

    from November 25, 2008 saying this is not possible in Eagle 4 and

    5.

     

    Is this possible in Eagle 6.2?

     

    --- Graham

     

    ==

     

     

     

     

    Graham,

     

    the situation in EAGLE 6 is the same as it was in version 4 or 5.

    The pad diameter always obeys at least the minimum value that is

    given for the width of the copper ring around the drilling in the

    Design Rule's restring settings.

     

     

    My solution to this is to NEVER use the auto diameter.  The first thing I

    do in a new PCB is set the minimum rest-ring to 0 and the max to 9999 (or

    some really large number).  By doing that, the DRC will simply use the

    diameter given in the library or set explicitly for a given via or pad

    object.

     

    To me, it doesn't make much sense to be using the same percentage for

    rest-ring on 0.008" drills as for 0.150" drills.  To get a manufacturable

    0.008" drill pad the size of the pads for the large holes is huge.  For

    mounting holes you might want this, but not always.

     

    So my solution is to NEVER use the auto diameter.  Just be careful.  Any

    via that gets through with the diameter set to auto will end up with a

    zero-sized rest-ring.  I've been meaning to write a ULP to detect diameter

    sizes set to auto, I just haven't got around to that yet.

     

    Cheers,

     

    James.

    --

    James Morrison  ~~~  Stratford Digital

     

    Specializing in CadSoft EAGLE

    • Online Sales to North America

    • Electronic Design Services

    • EAGLE Enterprise Toolkit

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.