Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Storing custom made lbr files
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 189 subscribers
  • Views 1799 views
  • Users 0 members are here
Related

Storing custom made lbr files

StefanTh
StefanTh over 13 years ago

Hi

 

I have both EAGLE-6.2.0 and EAGLE-6.3.0 installed on my Windows 7 platform.

Over the time I have made a number of .lbr files with both EAGLE versions.

Nowdays I only use EAGLE-6.3.0.

I create designs with components form libraries I have created with both versions of EAGLE.

The parameter "Libraries" in the "Directory" menu is set to "$EAGLEDIR\lbr"

 

Do a newer EAGLE version search older installed EGALE versions /lbr directory for .lbr files ?

Do EAGLE "move around" custom made .lbr files when it is installed ?

 

If a do a search for one of my files, hartman.lbr, I can not find it, neither in C:\Program Files (x86)\EAGLE-6.2.0 or in C:\Program Files (x86)\EAGLE-6.3.0 but if I do "Open library" in EAGLE-6.3.0 and move to C:\Program Files (x86)\EAGLE-6.2.0\lbr EAGLE it will find the file and I can open it ??

 

 

 

Regards Stefan

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Am 01.11.2012 08:09, schrieb Stefan Olsson:

    Hi

     

    I have both EAGLE-6.2.0 and EAGLE-6.3.0 installed on my Windows 7 platform.

    Over the time I have made a number of .lbr files with both EAGLE versions.

    Nowdays I only use EAGLE-6.3.0.

    I create designs with components form libraries I have created with both versions of EAGLE.

    The parameter "Libraries" in the "Directory" menu is set to "$EAGLEDIR\lbr"

     

    Do a newer EAGLE version search older installed EGALE versions /lbr directory for .lbr files ?

    Do EAGLE "move around" custom made .lbr files when it is installed ?

     

    If a do a search for one of my files, hartman.lbr, I can not find it, neither in C:\Program Files (x86)\EAGLE-6.2.0 or in C:\Program Files (x86)\EAGLE-6.3.0 but if I do "Open library" in EAGLE-6.3.0 and move to C:\Program Files (x86)\EAGLE-6.2.0\lbr EAGLE it will find the file and I can open it ??

     

    >

     

    Regards Stefan

     

     

    Eagle-6.3.0 is a newer version and may contain updated libraries and

    some other corrections.

    If you have created your own devices you should put them into your own

    libraries and place them into a different directory.

    Otherwise if you update eagle into the same directory the libraries will

    be overwritten and your work is lost.

    You must add the path to your own libraries in the control panel

    /options /directories and separate it from existing entry by a semicolon.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • StefanTh
    StefanTh over 13 years ago in reply to e14 Contributor

    Hi

     

    I do understand that and I try to archive this, but I can not find the files I have created, but EAGLE do.

     

    An example.

     

    I have created a library, hartman.lbr:

     

    This library I can open up within EAGLE by doing doing "Open library" but when I try to find the actual file it is nowhere to be found,

     

    neither in

    C:\Program Files (x86)\EAGLE-6.2.0\lbr

    or in

    C:\Program Files (x86)\EAGLE-6.3.0\lbr

     

    So, my question is/was, is EAGLE moving the library files around on it's own, do it concatenate library files when newer versions of EAGLE is installed etc.

     

     

    Reagrds

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to StefanTh

    Am 01.11.2012 09:36, schrieb Stefan Olsson:

    Hi

     

    I do understand that and I try to archive this, but I can not find the files I have created, but EAGLE do.

     

    An example.

     

    I have created a library, hartman.lbr:

     

    This library I can open up within EAGLE by doing doing "Open library" but when I try to find the actual file it is nowhere to be found,

     

    neither in

    C:\Program Files (x86)\EAGLE-6.2.0\lbr

    or in

    C:\Program Files (x86)\EAGLE-6.3.0\lbr

     

    So, my question is/was, is EAGLE moving the library files around on it's own, do it concatenate library files when newer versions of EAGLE is installed etc.

     

    >

    Reagrds

     

     

    No, why should eagle?

    The variable $EAGLEDIR depends on system. Why don't you set a real path?

    If you can open your "hartman.lbr" from an eagle sheet/board you should

    be able to move up the path to your actual directory.

    If this doesn't work start a file search with your operating systen.

    Also check that the library is "in use".

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    OK, so along the lines of what Richard says (and others have mentioned),

    you user modified/created libs should be somewhere else the user has access

    to.  Does anyone have a preferred data structure ?  I notice in W7, when

    Eagle 6.3 is installed, it creates a default location for projects under

    the users path ( C:\Users\mikey\Documents\eagle\ ).  Two questions come up

    in my mind since I am just getting things setup on my machine - is it best

    to create a "libs" folder under the C:\Users\mikey\Documents\eagle\ path (

    C:\Users\mikey\Documents\eagle\my-libs for example)?  How about 3rd party

    libraries like the sparkfun or adafruit libs - put them in the same

    "my-libs" folder or put them in a different folder (but still under the

    users path)?  What has worked best for folks ?  I realize that in the past

    many people just put them in the same library as the Eagle installed libs,

    however, as we have seen, that is not a good plan (and Windows is working

    to help us figure a better plan) for a number of reasons. It would be nice

    to have a consensus on where to put extra libs.

     

    When you add a folder to the search path for libs in eagle, does it just

    search that folder or does it search sub-folders within that specified

    folder ?

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Definitely agree with Richard's comment.  Best solution is to have your own

    libraries in your own user space and as he suggests, leave the Eagle

    libraries as read-only.  One thing that I think could be helpful is for the

    Eagle install process to put a 00_README.txt file in the library directory

    briefly describing this issue and the suggested way of storing libraries -

    from my searching, I have found many folks that a) don't know the best way

    to edit library parts and b) are not sure where to put libraries they have

    created.  The UAC thing is certainly not Eagles problem, but it does catch

    people un-aware who are used to older versions of windows or other OS's

    since the problem comes down to the files not being where you think they

    are (like soft links in the Unix world).

     

    mikey

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Hello,

     

    The UAC Virtualization is of course not an Eagle issue. It's Microsoft 

    doing it's best to integrate into W7 a way of working that was (sort of) 

    allowed in older Windows versions. It's debatable wether it's the best way 

    to do it but let's not start that here....

     

    As a word of advice: use the supplied Eagle lib's as 'read only'. That is, 

    as soon as you use a component from one of those lib's, copy it to your 

    own lib. NEVER modify the suplied lib's. Those lib's are updated when 

    needed and you can bet that by that time you can't remember which library 

    you modified and want to keep and which are ok to update. It could even be 

    that, for some reason, the part you used isn't in the updated lib.

     

    To avoid a lot of headache in the future, make you own lib's. To make it 

    easier, you can use the same name as the Cadsoft lib, prepended by 

    something (diode.lbr > own_diode.lbr). It will save you the trouble of 

    having to think of a lot of funky names..

     

    Place those lib's somewhere where a normal user has write access and add 

    the path to the directory setup in the Eagle control panel (first entry; 

    Eagle searches lib's in the order they are written down here). If you use 

    the Cadsoft lib's this way, you can leave them where they are.

     

     

    Richard

     

     

    Op Sat, 03 Nov 2012 06:22:36 +0100 schreef Mike Fields 

    <mr.gadget2@comcast.net>:

     

    I thought you were confused, but you seem to have it figured out "You are

    not allowed to write to this area, but you can actually, but not here, 

    but

    it looks like it, you can do it but virtualized, if this manifest file

    exist or if the launcher is UAC aware or starter program is

    elevated........"  man that one is confusing.  I think I want my old CP/M

    system back with the floppy drives and a 4mhz Z-80.  Also new to Eagle, 

    I'm

    going to have to be careful to avoid that trap door and make sure I have

    any of my libraries in my local directory with the preferences pointing 

    to

    it.  Thanks for finding that tidbit.

     

    mikey

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to StefanTh

    I thought you were confused, but you seem to have it figured out "You are

    not allowed to write to this area, but you can actually, but not here, but

    it looks like it, you can do it but virtualized, if this manifest file

    exist or if the launcher is UAC aware or starter program is

    elevated........"  man that one is confusing.  I think I want my old CP/M

    system back with the floppy drives and a 4mhz Z-80.  Also new to Eagle, I'm

    going to have to be careful to avoid that trap door and make sure I have

    any of my libraries in my local directory with the preferences pointing to

    it.  Thanks for finding that tidbit.

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to StefanTh

    I thought you were confused, but you seem to have it figured out "You are

    not allowed to write to this area, but you can actually, but not here, but

    it looks like it, you can do it but virtualized, if this manifest file

    exist or if the launcher is UAC aware or starter program is

    elevated........"  man that one is confusing.  I think I want my old CP/M

    system back with the floppy drives and a 4mhz Z-80.  Also new to Eagle, I'm

    going to have to be careful to avoid that trap door and make sure I have

    any of my libraries in my local directory with the preferences pointing to

    it.  Thanks for finding that tidbit.

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    OK, so along the lines of what Richard says (and others have mentioned),

    you user modified/created libs should be somewhere else the user has access

    to.  Does anyone have a preferred data structure ?  I notice in W7, when

    Eagle 6.3 is installed, it creates a default location for projects under

    the users path ( C:\Users\mikey\Documents\eagle\ ).  Two questions come up

    in my mind since I am just getting things setup on my machine - is it best

    to create a "libs" folder under the C:\Users\mikey\Documents\eagle\ path (

    C:\Users\mikey\Documents\eagle\my-libs for example)?  How about 3rd party

    libraries like the sparkfun or adafruit libs - put them in the same

    "my-libs" folder or put them in a different folder (but still under the

    users path)?  What has worked best for folks ?  I realize that in the past

    many people just put them in the same library as the Eagle installed libs,

    however, as we have seen, that is not a good plan (and Windows is working

    to help us figure a better plan) for a number of reasons. It would be nice

    to have a consensus on where to put extra libs.

     

    When you add a folder to the search path for libs in eagle, does it just

    search that folder or does it search sub-folders within that specified

    folder ?

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Definitely agree with Richard's comment.  Best solution is to have your own

    libraries in your own user space and as he suggests, leave the Eagle

    libraries as read-only.  One thing that I think could be helpful is for the

    Eagle install process to put a 00_README.txt file in the library directory

    briefly describing this issue and the suggested way of storing libraries -

    from my searching, I have found many folks that a) don't know the best way

    to edit library parts and b) are not sure where to put libraries they have

    created.  The UAC thing is certainly not Eagles problem, but it does catch

    people un-aware who are used to older versions of windows or other OS's

    since the problem comes down to the files not being where you think they

    are (like soft links in the Unix world).

     

    mikey

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Hello,

     

    The UAC Virtualization is of course not an Eagle issue. It's Microsoft 

    doing it's best to integrate into W7 a way of working that was (sort of) 

    allowed in older Windows versions. It's debatable wether it's the best way 

    to do it but let's not start that here....

     

    As a word of advice: use the supplied Eagle lib's as 'read only'. That is, 

    as soon as you use a component from one of those lib's, copy it to your 

    own lib. NEVER modify the suplied lib's. Those lib's are updated when 

    needed and you can bet that by that time you can't remember which library 

    you modified and want to keep and which are ok to update. It could even be 

    that, for some reason, the part you used isn't in the updated lib.

     

    To avoid a lot of headache in the future, make you own lib's. To make it 

    easier, you can use the same name as the Cadsoft lib, prepended by 

    something (diode.lbr > own_diode.lbr). It will save you the trouble of 

    having to think of a lot of funky names..

     

    Place those lib's somewhere where a normal user has write access and add 

    the path to the directory setup in the Eagle control panel (first entry; 

    Eagle searches lib's in the order they are written down here). If you use 

    the Cadsoft lib's this way, you can leave them where they are.

     

     

    Richard

     

     

    Op Sat, 03 Nov 2012 06:22:36 +0100 schreef Mike Fields 

    <mr.gadget2@comcast.net>:

     

    I thought you were confused, but you seem to have it figured out "You are

    not allowed to write to this area, but you can actually, but not here, 

    but

    it looks like it, you can do it but virtualized, if this manifest file

    exist or if the launcher is UAC aware or starter program is

    elevated........"  man that one is confusing.  I think I want my old CP/M

    system back with the floppy drives and a 4mhz Z-80.  Also new to Eagle, 

    I'm

    going to have to be careful to avoid that trap door and make sure I have

    any of my libraries in my local directory with the preferences pointing 

    to

    it.  Thanks for finding that tidbit.

     

    mikey