I'm using Eagle 6.3 (this problem occurred in 6.2 also). I'm trying to
find a way to display all components of the same value. I found a script
"ShowVals.ulp" which is supposed to do this, but it doesn't work. I later
found "find.ulp" which comes with Eagle, but that doesn't work either.
In both cases, the script(s) run, but the components are not highlighted.
In trying to debug the problem I noticed that I cannot even get a simple
"SHOW" command to work inside a script.
For example: having a file called test.scr and putting the line
Show U1
Does nothing. If I type the exact same command into the command line, it
works as expected. If I put "info U1", into the script, it runs the info
command as expected, so I know the script file and interface are working.
Trying "RUN find U1 -S" does nothing.
Is there any way to successfully use the "SHOW" command within a script?
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.