Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) How to Route 0.1 inch and 0.5mm devices
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 373 views
  • Users 0 members are here
Related

How to Route 0.1 inch and 0.5mm devices

e14 Contributor
e14 Contributor over 13 years ago

I have a design which contains 5 0.1 inch pitch connector

   pinhead -> pinhd2x5

and a 0.5mm pitch connector,

   con-hirose -> FH12-50S-0.5SH

 

and, some 74xxx smd devices.

 

The autorouter will route the pinhd2x5 and the 74xxx smd devices, but,

not the FH12-50S-0.5SH.

 

How do I do this?

 

Tom Dean

 

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Joern Paschedag wrote:

    Am 03.11.2012 01:13, schrieb Thomas D. Dean:

    >> I have a design which contains 5 0.1 inch pitch connector

    >>    pinhead -> pinhd2x5

    >> and a 0.5mm pitch connector,

    >>    con-hirose -> FH12-50S-0.5SH

    >>

    >> and, some 74xxx smd devices.

    >>

    >> The autorouter will route the pinhd2x5 and the 74xxx smd devices,

    >> but, not the FH12-50S-0.5SH.

    >>

    >> How do I do this?

    >>

    >> Tom Dean

     

    The autorouter is allways on grid, so make the grid smaller.

    If you want manually route off grid connections then start at the off

    grid point because eagle snaps to this point automatically and route

    at least to the nearest grid.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    Joern is referring to the autorouter grid which is different to the grids

    you use in the design editor .

     

    The manual explains it well. (in the .docs folder) From the explanation you

    can understand you must select an appropriate routing grid for the

    autorouter otherwise it will not route to some pins or route between pins

    when there is space to do it.

     

    HTH

    Warren

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    Am 03.11.2012 01:13, schrieb Thomas D. Dean:

    I have a design which contains 5 0.1 inch pitch connector

       pinhead -> pinhd2x5

    and a 0.5mm pitch connector,

       con-hirose -> FH12-50S-0.5SH

     

    and, some 74xxx smd devices.

     

    The autorouter will route the pinhd2x5 and the 74xxx smd devices, but,

    not the FH12-50S-0.5SH.

     

    How do I do this?

     

    Tom Dean

     

    The autorouter is allways on grid, so make the grid smaller.

    If you want manually route off grid connections then start at the off

    grid point because eagle snaps to this point automatically and route at

    least to the nearest grid.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag